cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H5 Interface With Gigabit Ethernet PHY device

B.Michele
Associate III

Moved from MPUs forum.


Hi, i must Use a Single Port Gigabit Ethernet PHY  that have a RGMII Gigabit Interface to connect a RMII 10/100 Mbit
Ethernet MAC interface of the STM32H563VI MCU. 

Do you think it is possible to connect a Gigabit PHY chip to the 100 Mbit H5 micros??? pin out,

Sure the final Ethernet Speed of the system, will be declasses to 10/100 Mbit. 

In particular I can't find where to connect the PA7 pin [RMII_CRS_DV] Carrier Sense... there is no CRS_DV output in the PHY gigabit device

 

Thank you very much

1 ACCEPTED SOLUTION

Accepted Solutions

Ok thank you,

we are also just looking for a newer chip than the LAN 8742, we will probably choose the Microchip or TI brand

View solution in original post

10 REPLIES 10
mƎALLEm
ST Employee

Hello,

STM32 MCUs don't support Ethernet Gigabit. Only MPU family does: STM32MP1xx, STM32MP2xx

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PatrickF
ST Employee

Not possible to connect RGMII PHY to an RMII interface. They are using different signals and clocks.

You need to look for a RMII PHY.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Good evening SofLit,

Thank you for your answer;  Yes I Know that STM32H563VI  MCU haven't the Gigabit Interface but only the 10/100 Mbit/s Fast Ethernet Like All H5-H7 ecc.. STM Arm processor
For me it' Ok to have only 100 Mbit/s speed  But I want Interface the PHY Phisical Layer to magnetic and RJ45 Copper Ethernet line With a New Chip Gigabit that have RGMII line.

So i want interface the RMII or MII Interface of STM H5 With a RGMII PHY Chip;

Is it possible to adapt the signals together with some I/O pins to drive the RGMII interface by downgrading it to max 100 Mbit??

Thank's

Good evening PatrickF,

Thank you for your answer;  Ok The H5 MCU haven't the RGMII but only  the SMI, MII, RMII, interface.

I was wondering if it's not really possible to adapt the signals together with some I/O pins to drive the RGMII interface by downgrading it to max 100 Mbit??   with the RMII Or MII H5 pinout and some other I/O pin.... 
downgrading the clock to 25 MHz I think, or whatever it takes....

Thank's

Hi, @B.Michele 

sorry to be rude, but I fear there is no way, they are too different.

RGMII PHY could run on 100Mbit/s link, but it is still using RGMII protocol.

Either you use an RMII PHY with STM32H5, or use an STM32 having RGMII capabilities (STM32N6, STM32MP1, STM32MP2 families).

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Pavel A.
Evangelist III

@B.Michele Please ask the vendor of the PHY if they support RMII. We have successfully connected STM32H753 to a 10/100/GB Broadcom switch chip, in 100 M RMII mode.

 

Thank you @PatrickF

Ok, thanks for the advice, so ultimately the "Copper" or "Fiber" Ethernet PHY device must support one of the two protocols of the H5: 'MII' or 'RMII'

The H5 MCU have only the MII and RMII Media Independent Interface that i must use. Together with the SMI serial signal realize the MAC interface for the PHY device.

-----

So the last question for reflection is that with a RMII MAC and a PHY that supports both copper and fiber I can achieve 100 Mbps with both magnetic and RJ45 and optical fiber?? with only RMII protocol ??

 

Thank's @PatrickF

Thank you @Pavel A.,

Thanks for your suggestion, certainly i see the opinion too with my MaxLinear Single Port Gigabit Ethernet PHY with RGMII Or SGMII interface.  H7 & H5 I think they have the same Ethernet MAC interface.
I can only ask you the brand of the PHY chips ??

Thank's

I can only ask you the brand of the PHY chips

For bring-up we used PHYs similar to LAN8742.