2025-02-07 02:45 AM - last edited on 2025-02-07 02:50 AM by Andrew Neil
Moved from MPUs forum.
Hi, i must Use a Single Port Gigabit Ethernet PHY that have a RGMII Gigabit Interface to connect a RMII 10/100 Mbit
Ethernet MAC interface of the STM32H563VI MCU.
Do you think it is possible to connect a Gigabit PHY chip to the 100 Mbit H5 micros??? pin out,
Sure the final Ethernet Speed of the system, will be declasses to 10/100 Mbit.
In particular I can't find where to connect the PA7 pin [RMII_CRS_DV] Carrier Sense... there is no CRS_DV output in the PHY gigabit device
Thank you very much
2025-02-13 01:15 AM
Ok thank you,
we are also just looking for a newer chip than the LAN 8742, we will probably choose the Microchip or TI brand