cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H5 Interface With Gigabit Ethernet PHY device

B.Michele
Associate III

Moved from MPUs forum.


Hi, i must Use a Single Port Gigabit Ethernet PHY  that have a RGMII Gigabit Interface to connect a RMII 10/100 Mbit
Ethernet MAC interface of the STM32H563VI MCU. 

Do you think it is possible to connect a Gigabit PHY chip to the 100 Mbit H5 micros??? pin out,

Sure the final Ethernet Speed of the system, will be declasses to 10/100 Mbit. 

In particular I can't find where to connect the PA7 pin [RMII_CRS_DV] Carrier Sense... there is no CRS_DV output in the PHY gigabit device

 

Thank you very much

10 REPLIES 10

Ok thank you,

we are also just looking for a newer chip than the LAN 8742, we will probably choose the Microchip or TI brand