2025-02-12 8:25 AM - last edited on 2025-02-12 8:39 AM by mƎALLEm
Moved from this thread.
ADC usage configuration.
I have a project that already uses pins PA4 and PA5 with the DAC, but I cannot obtain a value when using pin PA6 to read a voltage level
2025-02-12 8:21 AM - last edited on 2025-02-12 8:31 AM by Andrew Neil
Could you give me a simple solution?
2025-02-12 8:22 AM
What do you mean by simple solution?
2025-02-12 8:39 AM
Need to explain what do you mean by "I cannot obtain a value when using pin PA6 to read a voltage level"?
Always 0? constant value? else?
Need to attach your project so others can help you efficiently.
2025-02-12 8:44 AM
Always 0
I don't know if I'm configuring something wrong2025-02-12 8:45 AM
You need to share your code ..
2025-02-12 8:49 AM - last edited on 2025-02-12 8:58 AM by mƎALLEm
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
// uint8_t i = 0;
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
DAC_Init();
DAC_Start();
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DAC1_Init();
MX_I2C1_Init();
MX_USART2_UART_Init();
MX_TIM2_Init();
MX_ADC2_Init();
/* USER CODE BEGIN 2 */
ssd1306_Init();
ssd1306_Fill(Black);
ssd1306_UpdateScreen();
HAL_TIM_Base_Start_IT(&htim2);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
Menu_Select(select_position, select_mod);
while (1){
set_period = ((1.0 / frequency) * 1000000)/10;
uint32_t adc_value = readADC();
// float voltage_measured = (adc_value * 4.2) / 4095.0;
// if (voltage_measured <= 3.9) {
// status = 1;
// }
// else if (voltage_measured >= 3.9 && voltage_measured < 4.1) {
// status = 2;
// } else {
// status = 3;
// }
}
}
static void MX_DAC1_Init(void)
{
/* USER CODE BEGIN DAC1_Init 0 */
/* USER CODE END DAC1_Init 0 */
DAC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN DAC1_Init 1 */
/* USER CODE END DAC1_Init 1 */
/** DAC Initialization
*/
hdac1.Instance = DAC1;
if (HAL_DAC_Init(&hdac1) != HAL_OK)
{
Error_Handler();
}
/** DAC channel OUT1 config
*/
sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/** DAC channel OUT2 config
*/
if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN DAC1_Init 2 */
/* USER CODE END DAC1_Init 2 */
}
static void MX_ADC2_Init(void)
{
/* USER CODE BEGIN ADC2_Init 0 */
/* USER CODE END ADC2_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC2_Init 1 */
/* USER CODE END ADC2_Init 1 */
/** Common config
*/
hadc2.Instance = ADC2;
hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc2.Init.Resolution = ADC_RESOLUTION_12B;
hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc2.Init.ContinuousConvMode = DISABLE;
hadc2.Init.DiscontinuousConvMode = DISABLE;
hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc2.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc2.Init.NbrOfConversion = 1;
hadc2.Init.DMAContinuousRequests = ENABLE;
hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc2.Init.LowPowerAutoWait = DISABLE;
hadc2.Init.Overrun = ADC_OVR_DATA_PRESERVED;
if (HAL_ADC_Init(&hadc2) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_3; // PA6 = ADC2_IN3
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_601CYCLES_5; // Tempo de amostragem rápido
if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC2_Init 2 */
/* USER CODE END ADC2_Init 2 */
}
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, BRIDGE_H_CH1_1_Pin|BRIDGE_H_CH1_2_Pin|BRIDGE_H_CH2_2_Pin|BRIDGE_H_CH2_1_Pin, GPIO_PIN_RESET);
/*Configure GPIO pins : BT_DOWN_CH2_Pin BT_UP_CH2_Pin */
GPIO_InitStruct.Pin = BT_DOWN_CH2_Pin|BT_UP_CH2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*Configure GPIO pins : BRIDGE_H_CH1_1_Pin BRIDGE_H_CH1_2_Pin BRIDGE_H_CH2_2_Pin BRIDGE_H_CH2_1_Pin */
GPIO_InitStruct.Pin = BRIDGE_H_CH1_1_Pin|BRIDGE_H_CH1_2_Pin|BRIDGE_H_CH2_2_Pin|BRIDGE_H_CH2_1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : BT_UP_SELECT_Pin BT_DOWN_SELECT_Pin BT_SELECT_Pin BT_START_STOP_Pin */
GPIO_InitStruct.Pin = BT_UP_SELECT_Pin|BT_DOWN_SELECT_Pin|BT_SELECT_Pin|BT_START_STOP_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pins : BT_UP_CH1_Pin BT_DOWN_CH1_Pin */
GPIO_InitStruct.Pin = BT_UP_CH1_Pin|BT_DOWN_CH1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
2025-02-12 8:49 AM - last edited on 2025-02-12 8:53 AM by mƎALLEm
uint32_t readADC(void) {
uint32_t adcValue = 0;
HAL_ADC_Start(&hadc2); // Inicia a conversão
// if (HAL_ADC_PollForConversion(&hadc2, 10) == HAL_OK) {
// adcValue = HAL_ADC_GetValue(&hadc2); // Obtém o valor convertido
// }
adcValue = HAL_ADC_GetValue(&hadc2); // Obtém o valor convertido
HAL_ADC_Stop(&hadc2); // Para o ADC após a leitura
return adcValue;
}
2025-02-12 8:57 AM - edited 2025-02-12 8:59 AM
@Felipe_Nascimento wrote:
uint32_t readADC(void) { uint32_t adcValue = 0; HAL_ADC_Start(&hadc2); // Inicia a conversão // if (HAL_ADC_PollForConversion(&hadc2, 10) == HAL_OK) { // adcValue = HAL_ADC_GetValue(&hadc2); // Obtém o valor convertido // } adcValue = HAL_ADC_GetValue(&hadc2); // Obtém o valor convertido HAL_ADC_Stop(&hadc2); // Para o ADC após a leitura return adcValue; }
You need also to provide the ADC configuration as well as the DAC + their GPIO configs
Meanwhile, you need to poll on the end of the conversion + you need to calibrate the ADC before to start. From the HAL example:
if (HAL_ADCEx_Calibration_Start(&AdcHandle_slave, ADC_SINGLE_ENDED) != HAL_OK)
PS: please use </> button to paste your code. See this link.