2022-10-10 03:56 AM
From the datasheet PA0 is listed as a 5V tolerant IO (FT type).
Does this maximum of 5V still hold if the pin is mapped to the ADC input? If not, what is the maximum reading for this case?
Solved! Go to Solution.
2022-10-10 05:24 AM
According to the Reference Manual section 8.3.12 "Analog configuration"
In the analog configuration, the I/O pins cannot be 5 Volt tolerant.
In this case I would expect the maximum to be Vdd. (Strictly speaking Vdd + 0.3 V).
Hope this helps,
Danish
2022-10-10 05:24 AM
According to the Reference Manual section 8.3.12 "Analog configuration"
In the analog configuration, the I/O pins cannot be 5 Volt tolerant.
In this case I would expect the maximum to be Vdd. (Strictly speaking Vdd + 0.3 V).
Hope this helps,
Danish
2022-10-10 08:08 AM
There's also footnote (5) to the pin definitions table, saying
FT = 5 V tolerant except when in analog mode or oscillator mode (for PC14, PC15, PH0 and PH1).
> In this case I would expect the maximum to be Vdd. (Strictly speaking Vdd + 0.3 V).
Strictly speaking VDDA+0.3V, but in 'F4 there's also a requirement for VDDA=VDD.
JW