2023-10-11 09:21 AM
This is not true, according to RM, HSE is divided by RCC_CFGR.RTCPRE which ranges from HSE/2 to HSE/31.
JW
2023-10-11 09:50 AM
Hello @waclawek.jan,
Thank you for bringing up this issue
I can already confirm that the information in the datasheet is not totally coherent with the RTC block diagram (HSE/32):
I will further look into this issue and get back to you asap
Thank you!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-12 05:44 AM
Hi @Sarra.S ,
Indeed, a third divider, wrong again.
I understand that it's consequence of copy/paste, but it deserves to be cleaned up.
Thanks,
Jan
2023-10-12 07:20 AM
Hello again @waclawek.jan,
I can confirm that The correct description is in RCC so from HSE/2 to HSE/31.
This issue is tracked internally to be corrected (Ticket 163728).
Thank you for bringing up this issue.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.