cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 with small flash + HAL + DEBUG + no Optimization...

LCE
Principal

... leads to "funny" results:

STM32L011 with 16 kB of flash, HAL inits and LED toggle in main, DEBUG, no optimization:

93% of flash used

I had not expected it to be that bad! 

Okay, I will probably not use too much HAL, will use Release version with optimization,
but I better select an L01 in the next bigger QFN package (4x4) to get 32 kB of flash.

STM32L011_HAL_DEBUG_noOpt.png

21 REPLIES 21
MM..1
Chief II

Your screenshot show many peripherals , then maybe your LED toggle count bitcoins too ...

 

Andrew Neil
Evangelist III

Show the results with "Optimise for Debug" (-Og).

You should also take a look at the map file - is it actually HAL that's using all that space ... ?

KnarfB
Principal III

The Memory Details tab gives you more insights.

hth

KnarfB

LCE
Principal

Yes, luckily I know all that - it was just a bad surprise and might deter some complete STM32 beginners.

So, this wasn't actually a call for help, just ... being "amazed" at how things are. Until now I only worked with "bigger" STM32 (G4, F7, H7), and occasionally using HAL or at project start wasn't a problem.

 

The list file showed mostly the "bloated" HAL inits - I actually forgot about the "Memory Details", thanks @KnarfB .

With release / optimization to size, it drops to 56%.

Record holder is HAL_RCC_Config with 1.15 kB, together with HAL_RCC_ClockConfig and HAL_RCCEx_PeriphCLKConfig taking up even more than 10% of the 16 kB.
These are the HAL setup functions I always use - I guess I have to overcome my laziness in that area.

 

image.png

 

BTW - RAM: the default CubeMx settings for heap and stack also took up ~90%

 

In MX you can very easy switch some parts to LL

LCE
Principal

If this MCU will be used in a product, I will probably throw out the HAL stuff anyway (I don't like the LL either, so direct register settings for me).

I was just really shocked that a basically empty project - except for the inits - with all defaults from CubeMX leads to this memory usage: > 90% for flash and RAM.


@LCE wrote:

I was just really shocked that a basically empty project - except for the inits.


Probably, the inits are where 90% of the code lies!

So what do you get if you don't init any peripherals?

And then there's the C runtime support - how much did that amount to?

LCE
Principal

@Andrew Neil 

Probably, the inits are where 90% of the code lies!

Definitely!

I just switched to its next big brother with 32 kB SRAM, switched all to LL instead of HAL.

Release with no Opt: 9.57 kB flash

Release with Opt for size: 4.14 kB flash  <- I hadn't expected that with LL

 

And then there's the C runtime support - how much did that amount to?

Erm... where's that? Isn't that for memory allocation and stuff like that - which I don't use?


@LCE wrote:

@Andrew Neil 

Erm... where's that? Isn't that for memory allocation and stuff like that - which I don't use?


There's a lot more to it than that!