Genuine STLINK-V3MINIE doesn't work, but clone STLINK-V2 works
- March 30, 2025
- 31 replies
- 3757 views
I'm trying to make genuine STLINK-V3MINIE to work, but without success.
The target device is STM32F103C8T6.
VCC is connected to T_VCC (pin 3 of STDC14)
SWCLK is connected to T_SWCLK (pin 6 of STDC14)
SWDIO is connected to T_SWDIO (pin 4 of STDC14)
RESET is connected to T_NRST (pin 12 of STDC14)
GND is connected to GND and GNDDetect (pins 5, 7, 11 of STDC14)
STM32CubeProgrammer is properly detecting STLINK-V3MINIE, even shows voltage of the target.
But when I try to connect to target, it gives message:
Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
This is text from console:
12:56:46:283 : UR connection mode is defined with the HWrst reset mode
12:56:46:837 : ST-LINK SN : [redacted]
12:56:46:838 : ST-LINK FW : V3J16M7
12:56:46:838 : Board : STLINK-V3MINIE
12:56:46:838 : Voltage : 3.29V
12:56:46:839 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
12:56:46:876 : Disconnected
I tried another PC, but with the same result.
When I connect clone STLINK-V2 instead of genuine STLINK-V3MINIE, I'm able to connect to target MCU, and download program to target.
This is the output from console:
13:00:39:502 : UR connection mode is defined with the HWrst reset mode
13:00:39:667 : ST-LINK SN : [redacted]
13:00:39:667 : ST-LINK FW : V2J45S7
13:00:39:667 : Board : --
13:00:39:667 : Voltage : 3.18V
13:00:39:667 : SWD freq : 4000 KHz
13:00:39:667 : Connect mode: Normal
13:00:39:667 : Reset mode : Hardware reset
13:00:39:668 : Device ID : 0x410
13:00:39:668 : Revision ID : --
13:00:39:668 : flash loader C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0x410.stldr is loaded
13:00:39:668 : Debug in Low Power mode is not supported for this device.
13:00:39:668 : Reading data...
13:00:39:668 : r ap 0 @0x1FFFF7E0 0x00000004 bytes Data 0x00140040
13:00:39:957 : UPLOADING OPTION BYTES DATA ...
13:00:39:957 : Bank : 0x00
13:00:39:957 : Address : 0x4002201c
13:00:39:957 : Size : 8 Bytes
13:00:39:958 : Reading data...
13:00:39:958 : r ap 0 @0x4002201C 0x00000008 bytes Data 0x03FFFFFC
13:00:39:959 : Bank : 0x01
13:00:39:959 : Address : 0x1ffff800
13:00:39:959 : Size : 16 Bytes
13:00:39:959 : Reading data...
13:00:39:959 : r ap 0 @0x1FFFF800 0x00000010 bytes Data 0xFFFF5AA5
13:00:39:960 : UPLOADING OPTION BYTES DATA ...
13:00:39:960 : Bank : 0x00
13:00:39:960 : Address : 0x4002201c
13:00:39:960 : Size : 8 Bytes
13:00:39:960 : Reading data...
13:00:39:961 : r ap 0 @0x4002201C 0x00000008 bytes Data 0x03FFFFFC
13:00:39:961 : Bank : 0x01
13:00:39:961 : Address : 0x1ffff800
13:00:39:961 : Size : 16 Bytes
13:00:39:962 : Reading data...
13:00:39:962 : r ap 0 @0x1FFFF800 0x00000010 bytes Data 0xFFFF5AA5
13:00:39:962 : UPLOADING ...
13:00:39:962 : Size : 1024 Bytes
13:00:39:963 : Address : 0x8000000
13:00:39:963 : Read progress:
13:00:39:963 : Reading data...
13:00:39:964 : r ap 0 @0x08000000 0x00000400 bytes Data 0x20005000
13:00:39:964 : Data read successfully
13:00:39:964 : Time elapsed during the read operation is: 00:00:00.007
What is the problem with STLINK-V3MINIE?
How to make it work?
It's pretty frustrating that clone works and genuine debugger not.