cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 + eth phy with ieee1588

Pilous Droip
Senior

hi everyone,

Does stm32 have any ptp integration manual? For example, I would like to use a DP83640 with an integrated ieee1588. And this phy contains PTP/SFD interrupt pins. Are there any pins in stm32h7 family or stm32f7 family for this interrupt? Or do I join any interrupt gpio and create my own routine? Or how to successfully implement ptp on stm32?

 

 

2 REPLIES 2
mƎALLEm
ST Employee

See these threads as they may help you:

https://community.st.com/t5/stm32-mcus-embedded-software/ptp-support-in-hal-drivers-stm32h7/td-p/295602

https://community.st.com/t5/stm32-mcus-embedded-software/getting-started-with-ptp-ieee-1588/td-p/92965

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thanks for the links. What I didn't find anywhere, if for IEEE1588 implementations it is necessary to have an eth phy with the integration of this protocol or a simple DP83826 is enough or a DP83640 is needed?

 

So my question is, are both DP83826 and DP83640 suitable for STM32F7orH7 to implement IEEE1588?

https://www.ti.com/product/DP83826E

https://www.ti.com/product/DP83640