cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 + eth phy with ieee1588

Pilous Droip
Senior

hi everyone,

Does stm32 have any ptp integration manual? For example, I would like to use a DP83640 with an integrated ieee1588. And this phy contains PTP/SFD interrupt pins. Are there any pins in stm32h7 family or stm32f7 family for this interrupt? Or do I join any interrupt gpio and create my own routine? Or how to successfully implement ptp on stm32?

 

 

2 REPLIES 2
SofLit
ST Employee

See these threads as they may help you:

https://community.st.com/t5/stm32-mcus-embedded-software/ptp-support-in-hal-drivers-stm32h7/td-p/295602

https://community.st.com/t5/stm32-mcus-embedded-software/getting-started-with-ptp-ieee-1588/td-p/92965

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Thanks for the links. What I didn't find anywhere, if for IEEE1588 implementations it is necessary to have an eth phy with the integration of this protocol or a simple DP83826 is enough or a DP83640 is needed?

 

So my question is, are both DP83826 and DP83640 suitable for STM32F7orH7 to implement IEEE1588?

https://www.ti.com/product/DP83826E

https://www.ti.com/product/DP83640