cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-U575 CAPTURE FAIL, is it a silicon level bug?

dhs
Senior

For the Nucleo-575ZI-Q, while in stop mode 2, I have the capture module enabled, I set CH1 IO Usage as input.

A square wave generator connected to PC1->LPTIM_CH1.
While the Micro is in stop mode 2 an indeterminate number of pulses trigger successive captures.
If the pulses on PC1 were odd CCR1 has the correct data.
If the pulses on PC1 were even CCR1 value doesn't updated at all.

Please note that all pulses arrive while STM32U575 is on stop mode.

 

I made a very short project isolating the problem, the RTC is used to exit stop mode 2 every second, when waking up only CRR1 is read and returns to stop mode 2.

 

 

 

void FM_MAIN_Main() { uint16_t capture = 0; HAL_LPTIM_IC_Start(&hlptim1, LPTIM_CHANNEL_1); __HAL_RCC_LPTIM1_CLKAM_ENABLE(); for (;;) { HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_SET); capture = LPTIM1->CCR1; FM_DEBUG_UartUint16(capture); HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_RESET); HAL_SuspendTick(); HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI); HAL_ResumeTick(); } } /** * @brief LPTIM1 Initialization Function * None * @retval None */ static void MX_LPTIM1_Init(void) { /* USER CODE BEGIN LPTIM1_Init 0 */ /* USER CODE END LPTIM1_Init 0 */ LPTIM_IC_ConfigTypeDef sConfig = {0}; /* USER CODE BEGIN LPTIM1_Init 1 */ /* USER CODE END LPTIM1_Init 1 */ hlptim1.Instance = LPTIM1; hlptim1.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC; hlptim1.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV1; hlptim1.Init.Trigger.Source = LPTIM_TRIGSOURCE_SOFTWARE; hlptim1.Init.Period = 65535; hlptim1.Init.UpdateMode = LPTIM_UPDATE_IMMEDIATE; hlptim1.Init.CounterSource = LPTIM_COUNTERSOURCE_INTERNAL; hlptim1.Init.Input1Source = LPTIM_INPUT1SOURCE_GPIO; hlptim1.Init.Input2Source = LPTIM_INPUT2SOURCE_GPIO; hlptim1.Init.RepetitionCounter = 0; if (HAL_LPTIM_Init(&hlptim1) != HAL_OK) { Error_Handler(); } sConfig.ICInputSource = LPTIM_IC1SOURCE_GPIO; sConfig.ICPrescaler = LPTIM_ICPSC_DIV1; sConfig.ICPolarity = LPTIM_ICPOLARITY_RISING; sConfig.ICFilter = LPTIM_ICFLT_CLOCK_DIV1; if (HAL_LPTIM_IC_ConfigChannel(&hlptim1, &sConfig, LPTIM_CHANNEL_1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN LPTIM1_Init 2 */ /* USER CODE END LPTIM1_Init 2 */ } /** * @brief RTC Initialization Function * None * @retval None */ static void MX_RTC_Init(void) { /* USER CODE BEGIN RTC_Init 0 */ /* USER CODE END RTC_Init 0 */ RTC_PrivilegeStateTypeDef privilegeState = {0}; /* USER CODE BEGIN RTC_Init 1 */ /* USER CODE END RTC_Init 1 */ /** Initialize RTC Only */ hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = 127; hrtc.Init.SynchPrediv = 255; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE; hrtc.Init.BinMode = RTC_BINARY_NONE; if (HAL_RTC_Init(&hrtc) != HAL_OK) { Error_Handler(); } privilegeState.rtcPrivilegeFull = RTC_PRIVILEGE_FULL_NO; privilegeState.backupRegisterPrivZone = RTC_PRIVILEGE_BKUP_ZONE_NONE; privilegeState.backupRegisterStartZone2 = RTC_BKP_DR0; privilegeState.backupRegisterStartZone3 = RTC_BKP_DR0; if (HAL_RTCEx_PrivilegeModeSet(&hrtc, &privilegeState) != HAL_OK) { Error_Handler(); } /** Enable the WakeUp */ if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_CK_SPRE_16BITS, 0) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN RTC_Init 2 */ /* USER CODE END RTC_Init 2 */ }
View more

 

 

 

dhs_0-1728412991039.png

dhs_1-1728413010046.png

 

Daniel H Sagarra
12 REPLIES 12

@Sarra.S In this project, I cannot use DMA. While the microcontroller is in stop mode 2, hundreds of captures can be produced, but only the last one is of interest to me. If the number of captures is odd, the value of the CCR1 register is correct; however, if the number of captures is even, the value of CCR1 fails and shows the last capture that occurred before entering stop mode.

Daniel H Sagarra

@Sarra.S 

How can I escalate this issue to another authority? The fault is very easy to replicate. I did it on several boards and with different processors, and the effect is disastrous for the quality of the microcontroller.

Daniel H Sagarra

Hello @dhs

I have escalated this case to the U5 team to further investigate (Internal ticket 197340). 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.