2024-10-11 12:10 PM
Hello Forum,
I have an issue while reading the values from ADC. ADC1 is running in "continues scan convertion mode" using DMA and 5 ranks.
Here is ADC_Init function:
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_MultiModeTypeDef multimode = {0};
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.GainCompensation = 0;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.NbrOfConversion = 5;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc1.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure the ADC multi-mode
*/
multimode.Mode = ADC_MODE_INDEPENDENT;
if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_TEMPSENSOR_ADC1;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_247CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_VREFINT;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_3;
sConfig.SamplingTime = ADC_SAMPLETIME_24CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_2;
sConfig.Rank = ADC_REGULAR_RANK_4;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_4;
sConfig.Rank = ADC_REGULAR_RANK_5;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */
/* USER CODE END ADC1_Init 2 */
}
Then, here is my main() function:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_DAC1_Init();
MX_I2C2_Init();
MX_USB_Device_Init();
MX_TIM17_Init();
MX_CRC_Init();
MX_ADC1_Init();
/* USER CODE BEGIN 2 */
if (HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED) != HAL_OK)
{
Error_Handler();
}
if (HAL_ADC_Start_DMA(&hadc1, (uint32_t *) &adc_convertions, 5) != HAL_OK)
{
Error_Handler();
}
HAL_DAC_Start(&hdac1, DAC1_CHANNEL_1);
HAL_DAC_Start(&hdac1, DAC1_CHANNEL_2);
HAL_TIM_Base_Start_IT(&htim17);
AT24CXX_Init(hi2c2);
load_configuration();
init_spline();
// load_default_configuration();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
timer_tasks_execute();
if (received_data)
{
process_tunerstudio();
received_data = false;
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
The variable adc_convertions is declared as uint32_t adc_convertions[5] = {0};
Issue:
If I apply the a voltage (2.15v) to PA1 and PA3, in adc_convertions array I get the ADC of 2620 for PA1 and 1531 for PA3. But, the both values shold be equal... The another ranks in adc_convertions array are correct.
So, 'Ive no idea anymore...
Can you please help me?
Many thanks & regards,
Heinrich
Solved! Go to Solution.
2024-10-11 11:44 PM - edited 2024-10-11 11:46 PM
> If I apply the a voltage (2.15v) to PA1 and PA3
So, are PA1 and PA3 physically connected together?
> I removed SB1 and SB12 (because PA3 is connected to STLINK-V3E virtual c omport)
And did you connect SB14?
JW
2024-10-11 12:40 PM
Change your type to uint16_t instead of uint32_t
2024-10-11 1:17 PM
Do you mean the type of adc_convertions[5]?
Regards,
Heinrich
2024-10-11 2:33 PM
Instead:
if (HAL_ADC_Start_DMA(&hadc1, (uint32_t *) &adc_convertions, 5) != HAL_OK)
try:
if (HAL_ADC_Start_DMA(&hadc1, (uint32_t *) adc_convertions, 5) != HAL_OK)
And declaration of : uint32_t adc_convertions[5] = {0}; depends on DMA_word size, what we can't see, since no dma config provided.
2024-10-11 11:44 PM - edited 2024-10-11 11:46 PM
> If I apply the a voltage (2.15v) to PA1 and PA3
So, are PA1 and PA3 physically connected together?
> I removed SB1 and SB12 (because PA3 is connected to STLINK-V3E virtual c omport)
And did you connect SB14?
JW
2024-10-12 2:21 AM
Yes ADC is 12bit then optimal result is 16bit half word DMA and uint16_t array.
And for addressing array right syntax is adc_convertions or &adc_convertions[0] .
2024-10-12 6:45 AM - edited 2024-10-12 6:46 AM
Hi guys, first of all, thank you very much for help :)
DMA is configured like this at the moment:
Since STM32 is a 32-bit MCU, WORD means uint32_t, I think... It is correct?
Yes, PA1 and PA3 are connected together. Not directly on Nucleo, but on carrier board. The is a voltage divider (5v to 3.3), then buffer and then NUCLEO. AI've applied 3.3v from NUCLEO to both input pins, after voltage diviers and buffers, I get 2.15v on BOTH pins of NUCLEO. So, the hardware should be okay, because the get the same voltage.
No, SB15 is still default, so not "installed".
@MM..1Okay, I've removed & , the DMA is configured as word, not half-word.
What I've done:
Result:
I will close SB14 a bit later and test it :)
2024-10-12 6:56 AM
If DMA configured as Word_Peripheral- Word_Memory, than
uint32_t adc_convertions[5] = {0}; or int32_t adc_convertions[5] = {0};
correct declaration.
For Halfword_Peripheral- Halfword_Memory, than
uint16_t adc_convertions[5] = {0}; or int16_t adc_convertions[5] = {0};
2024-10-12 7:23 AM
Okay, then it was correct.
I've changed them back to uint32_t adc_convertions[5] = {0};
and:
I'll test with SB14 closed today evening.
Regards,
Heinrich
2024-10-12 8:38 AM
sConfig.Channel = ADC_CHANNEL_VREFINT; sConfig.Rank = ADC_REGULAR_RANK_2;
why you mean this must equal RANK_1 ? And for effectivity set DMA to half word and array to uint16 ...