cancel
Showing results for 
Search instead for 
Did you mean: 

Incorrect ADC values when using HAL setup for DISCO-L475VG-IOT01A

mbe
Associate

The ADC values remain unchanged even when input signals does change. The C++ code provided below should hopefully clarify the situation, as I am a stuck. Thank you in advance for any help!

 

#include "mbed.h"
#include "stm32l4xx_hal.h"

//Once the buffer below is filled, transfer it over to the PC
#define ADC_BUF_SIZE 1024   // Number of samples in buffer
#define SAMPLE_RATE 50000   // Sampling rate in Hz (e.g., 50 kHz)

AnalogIn adc_pin(A0);  // Use A0 as the analog input pin

// ADC and DMA handles
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
uint16_t adc_buffer[ADC_BUF_SIZE];  // ADC DMA buffer
volatile bool buffer_ready = false; // Flag to indicate data is ready

void ADC_Init() {
    __HAL_RCC_ADC_CLK_ENABLE();       // Enable ADC Clock
    __HAL_RCC_DMA1_CLK_ENABLE();      // Enable DMA Clock
   
    hadc1.Instance = ADC1;
    hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
    hadc1.Init.Resolution = ADC_RESOLUTION_12B;
    hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
    hadc1.Init.ScanConvMode = DISABLE;
    hadc1.Init.ContinuousConvMode = ENABLE;
    hadc1.Init.DiscontinuousConvMode = DISABLE;
    hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
    hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
    hadc1.Init.DMAContinuousRequests = ENABLE;
    hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
   
    if (HAL_ADC_Init(&hadc1) != HAL_OK) {
        printf("ADC Init Failed!\n");
    }

    // Configure ADC Channel
    ADC_ChannelConfTypeDef sConfig = {0};
    sConfig.Channel = ADC_CHANNEL_5; // Corresponds to A0
    sConfig.Rank = ADC_REGULAR_RANK_1;
    sConfig.SamplingTime = ADC_SAMPLETIME_6CYCLES_5;  // Adjust if needed

    if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) {
        printf("ADC Channel Config Failed!\n");
    }
}

void DMA_Init() {
    // Configure DMA
    hdma_adc1.Instance = DMA1_Channel1;
    hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
    hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
    hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
    hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
    hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
    hdma_adc1.Init.Mode = DMA_CIRCULAR;
    hdma_adc1.Init.Priority = DMA_PRIORITY_HIGH;

    if (HAL_DMA_Init(&hdma_adc1) != HAL_OK) {
        printf("DMA Init Failed!\n");
    }

    __HAL_LINKDMA(&hadc1, DMA_Handle, hdma_adc1);

    // Enable Interrupt on DMA Transfer Complete
    HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 1, 0);
    HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
}

void Start_ADC_DMA() {
    HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adc_buffer, ADC_BUF_SIZE);
    printf("ADC Sampling Started...\n");
}

extern "C" void DMA1_Channel1_IRQHandler() {
    HAL_DMA_IRQHandler(&hdma_adc1);
}

// Callback function when buffer is full
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc) {
    if (hadc->Instance == ADC1) {
        buffer_ready = true;  // Signal that buffer is full
    }
}

void Process_ADC_Data() {
    if (buffer_ready) {
        buffer_ready = false;
        for (int i = 0; i < ADC_BUF_SIZE; i++) {
            printf("Sample %d: %d\n", i, adc_buffer[i]);
        }
    }
}

int main() {
    printf("Starting ADC DMA Sampling...\n");
   
    ADC_Init(); //
    DMA_Init(); //Direct memory access - giving permission to ADC to write into the memory
    Start_ADC_DMA(); //Start DMA writing
   
    while (1) {
        Process_ADC_Data();
        ThisThread::sleep_for(10ms);  // Avoid CPU overload
    }
}​

 


Code formatting applied - please see How to insert source code for future reference.



2 REPLIES 2
Saket_Om
ST Employee

Hello @mbe 

Could you check with ADC calibration before starting the conversion please? 

  /* Run the ADC calibration in single-ended mode */
  if (HAL_ADCEx_Calibration_Start(&AdcHandle, ADC_SINGLE_ENDED) != HAL_OK)
  {
    /* Calibration Error */
    Error_Handler();
  }

  /*##-3- Start the conversion process #######################################*/
  if (HAL_ADC_Start_DMA(&AdcHandle) != HAL_OK)
  {
    /* Start Conversation Error */
    Error_Handler();
  }
To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om
Andrew Neil
Super User

@mbe wrote:

The ADC values remain unchanged even when input signals does change.


Please give details of the input signal, and how it's connected.

Are you sure that the input signal is actually reaching the correct pin on the chip package?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.