2025-02-27 2:46 AM
Hello,
I have been trying for some days to read the values incoming form both ADCs, ADC1 & ADC4, from the NUCLEO U545-REQ.
The overall idea is to trigger both ADCs at the same time in output compare mode but if i try to trigger both of them at the same time in the live expression the read values are 0. I have tried to trigger the ADC4 in this mode and it works as expected.
I do not know the error i have. Find attached the configurations of the peripherals and the code:
I have the ADC4 configured as follows:
- Channels 3, 4, 9, 10, 11 in single ended mode
- Scan conversion mode is enabled
- DMA continuous request mode is enabled.
- External trigger conversion source is Timer 2 trigger Out event
- Trigger detection in rising edge
I have the ADC1 configured as follows:
- Channels 1, 2, 6, 7 in single ended mode
- Scan conversion mode is enabled
- DMA continuous request mode is enabled.
- External trigger conversion source is Timer 2 trigger Out event
- Trigger detection in rising edge
I have the Linked List configured as follows:
- Channel to run the linked list is GPDMA in circular mode and the first loop node is ADC1_Node.
- Two nodes are configured, ADC1_Node and ADC4_Node both with request parameter GPDMA1_REQUEST_ADC1 & GPDMA1_REQUEST_ADC4, direction is peripheral to memory in both nodes, data width is a word.
Timer 2 is configured as follows:
- Clock source: internal clock
- Channel 1 in Output Compare CH1
- Prescaler= 999
- Counter Period = 159999
- Trigger event selection TRGO: Output compare (OC1REF)
- Output compare channel 1:
- Mode: Toggle on match
- Pulse: 159999
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
COM_InitTypeDef BspCOMInit;
ADC_HandleTypeDef hadc1;
ADC_HandleTypeDef hadc4;
DMA_HandleTypeDef handle_GPDMA1_Channel10;
DMA_HandleTypeDef handle_GPDMA1_Channel8;
TIM_HandleTypeDef htim2;
/* USER CODE BEGIN PV */
uint32_t CNT_TIMER2 = 0;
uint32_t CCR_TIMER2 = 0;
uint32_t CCR_TIMER2_CONF = 0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void SystemPower_Config(void);
static void MX_GPIO_Init(void);
static void MX_GPDMA1_Init(void);
static void MX_ADC4_Init(void);
static void MX_ICACHE_Init(void);
static void MX_TIM2_Init(void);
static void MX_ADC1_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
#define ADC4_BUFFER_SIZE ((uint32_t) 5) // Buffer size ADC4
uint32_t ADC4_VALUES[ADC4_BUFFER_SIZE]; // Variable containing ADC4 conversions data
#define ADC1_BUFFER_SIZE ((uint32_t) 4) // Buffer size ADC1
uint32_t ADC1_VALUES[ADC1_BUFFER_SIZE]; // Variable containing ADC1 conversions data
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the System Power */
SystemPower_Config();
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_GPDMA1_Init();
MX_ADC4_Init();
MX_ICACHE_Init();
MX_TIM2_Init();
MX_ADC1_Init();
/* USER CODE BEGIN 2 */
MX_ADC_Queue_Config(); // Configuration of Queue
if(HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET_LINEARITY, ADC_SINGLE_ENDED)){ // ADC1 Calibration
Error_Handler();
}
__HAL_LINKDMA(&hadc1, DMA_Handle, handle_GPDMA1_Channel8);
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel8, &ADC_Queue) != HAL_OK)
{
Error_Handler();
}
if (HAL_ADC_Start_DMA(&hadc1, (uint32_t *)ADC1_VALUES, (ADC1_BUFFER_SIZE) ) != HAL_OK)
{
Error_Handler();
}
if(HAL_ADCEx_Calibration_Start(&hadc4, ADC_CALIB_OFFSET_LINEARITY, ADC_SINGLE_ENDED)){ // ADC4 Calibration
Error_Handler();
}
__HAL_LINKDMA(&hadc4, DMA_Handle, handle_GPDMA1_Channel10);
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel10, &ADC_Queue) != HAL_OK)
{
Error_Handler();
}
if (HAL_ADC_Start_DMA(&hadc4, (uint32_t *)ADC4_VALUES, (ADC4_BUFFER_SIZE) ) != HAL_OK)
{
Error_Handler();
}
HAL_TIM_OC_Start(&htim2, TIM_CHANNEL_1);
/* USER CODE END 2 */
/* Initialize led */
BSP_LED_Init(LED_GREEN);
/* Initialize USER push-button, will be used to trigger an interrupt each time it's pressed.*/
BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);
/* Initialize COM1 port (115200, 8 bits (7-bit data + 1 stop bit), no parity */
BspCOMInit.BaudRate = 115200;
BspCOMInit.WordLength = COM_WORDLENGTH_8B;
BspCOMInit.StopBits = COM_STOPBITS_1;
BspCOMInit.Parity = COM_PARITY_NONE;
BspCOMInit.HwFlowCtl = COM_HWCONTROL_NONE;
if (BSP_COM_Init(COM1, &BspCOMInit) != BSP_ERROR_NONE)
{
Error_Handler();
}
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
CNT_TIMER2= TIM2->CNT;
CCR_TIMER2_CONF= TIM2->CCR1;
__HAL_TIM_SET_COMPARE(&htim2, TIM_CHANNEL_1, (uint32_t) CCR_TIMER2);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_0;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV4;
RCC_OscInitStruct.PLL.PLLM = 3;
RCC_OscInitStruct.PLL.PLLN = 10;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 1;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief Power Configuration
* @retval None
*/
static void SystemPower_Config(void)
{
/*
* Switch to SMPS regulator instead of LDO
*/
if (HAL_PWREx_ConfigSupply(PWR_SMPS_SUPPLY) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN PWR */
/* USER CODE END PWR */
}
/**
* @brief ADC1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc1.Init.Resolution = ADC_RESOLUTION_14B;
hadc1.Init.GainCompensation = 0;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.NbrOfConversion = 4;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T2_TRGO;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
hadc1.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_12CYCLES;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_2;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_6;
sConfig.Rank = ADC_REGULAR_RANK_3;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_7;
sConfig.Rank = ADC_REGULAR_RANK_4;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */
/* USER CODE END ADC1_Init 2 */
}
/**
* @brief ADC4 Initialization Function
* @PAram None
* @retval None
*/
static void MX_ADC4_Init(void)
{
/* USER CODE BEGIN ADC4_Init 0 */
/* USER CODE END ADC4_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC4_Init 1 */
/* USER CODE END ADC4_Init 1 */
/** Common config
*/
hadc4.Instance = ADC4;
hadc4.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc4.Init.Resolution = ADC_RESOLUTION_12B;
hadc4.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc4.Init.ScanConvMode = ADC4_SCAN_ENABLE;
hadc4.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc4.Init.LowPowerAutoPowerOff = ADC_LOW_POWER_NONE;
hadc4.Init.LowPowerAutoWait = DISABLE;
hadc4.Init.ContinuousConvMode = DISABLE;
hadc4.Init.NbrOfConversion = 5;
hadc4.Init.DiscontinuousConvMode = DISABLE;
hadc4.Init.ExternalTrigConv = ADC4_EXTERNALTRIG_T2_TRGO;
hadc4.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
hadc4.Init.DMAContinuousRequests = ENABLE;
hadc4.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
hadc4.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc4.Init.SamplingTimeCommon1 = ADC4_SAMPLETIME_12CYCLES_5;
hadc4.Init.SamplingTimeCommon2 = ADC4_SAMPLETIME_12CYCLES_5;
hadc4.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc4) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_3;
sConfig.Rank = ADC4_REGULAR_RANK_1;
sConfig.SamplingTime = ADC4_SAMPLINGTIME_COMMON_1;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_4;
sConfig.Rank = ADC4_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_9;
sConfig.Rank = ADC4_REGULAR_RANK_3;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_10;
sConfig.Rank = ADC4_REGULAR_RANK_4;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_11;
sConfig.Rank = ADC4_REGULAR_RANK_5;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC4_Init 2 */
/* USER CODE END ADC4_Init 2 */
}
/**
* @brief GPDMA1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPDMA1_Init(void)
{
/* USER CODE BEGIN GPDMA1_Init 0 */
/* USER CODE END GPDMA1_Init 0 */
/* Peripheral clock enable */
__HAL_RCC_GPDMA1_CLK_ENABLE();
/* USER CODE BEGIN GPDMA1_Init 1 */
/* USER CODE END GPDMA1_Init 1 */
handle_GPDMA1_Channel10.Instance = GPDMA1_Channel10;
handle_GPDMA1_Channel10.InitLinkedList.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
handle_GPDMA1_Channel10.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
handle_GPDMA1_Channel10.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT0;
handle_GPDMA1_Channel10.InitLinkedList.TransferEventMode = DMA_TCEM_LAST_LL_ITEM_TRANSFER;
handle_GPDMA1_Channel10.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel10) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel10, DMA_CHANNEL_NPRIV) != HAL_OK)
{
Error_Handler();
}
handle_GPDMA1_Channel8.Instance = GPDMA1_Channel8;
handle_GPDMA1_Channel8.InitLinkedList.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
handle_GPDMA1_Channel8.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
handle_GPDMA1_Channel8.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT0;
handle_GPDMA1_Channel8.InitLinkedList.TransferEventMode = DMA_TCEM_LAST_LL_ITEM_TRANSFER;
handle_GPDMA1_Channel8.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel8) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel8, DMA_CHANNEL_NPRIV) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN GPDMA1_Init 2 */
/* USER CODE END GPDMA1_Init 2 */
}
/**
* @brief ICACHE Initialization Function
* @PAram None
* @retval None
*/
static void MX_ICACHE_Init(void)
{
/* USER CODE BEGIN ICACHE_Init 0 */
/* USER CODE END ICACHE_Init 0 */
/* USER CODE BEGIN ICACHE_Init 1 */
/* USER CODE END ICACHE_Init 1 */
/** Enable instruction cache in 1-way (direct mapped cache)
*/
if (HAL_ICACHE_ConfigAssociativityMode(ICACHE_1WAY) != HAL_OK)
{
Error_Handler();
}
if (HAL_ICACHE_Enable() != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ICACHE_Init 2 */
/* USER CODE END ICACHE_Init 2 */
}
/**
* @brief TIM2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 999;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 159999;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OC_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC1REF;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_TOGGLE;
sConfigOC.Pulse = 159998;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
/* USER CODE END TIM2_Init 2 */
HAL_TIM_MspPostInit(&htim2);
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
2025-02-27 4:10 AM
When you debug and run the code, does execution reach the main loop? What happens if you increase SamplingTime to max?
2025-02-27 5:41 AM
Thank you for the fast answer.
No, when debbuging it the execution does not reach the while loop.
It gets stuck in the following lines:
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel10, &ADC_Queue) != HAL_OK)
{
Error_Handler();
}Therefore the link between the ADC_Queue and the Channel 10 of the GPDMA is not well configured.
Heres the configuration of the GPDMA channels:
And heres the configuration of the ADC_Queue:
And the ADC_Nodes1(the ADC_Node4 is configured in the same way):
Is everything well configured?
If i increase the amount of sample time nothing changes.
2025-02-27 6:21 AM
Hello,
Debbuging the code the execution stops at the following part of the code:
if (pQList->State == HAL_DMA_QUEUE_STATE_BUSY)
{
/* Update the queue error code */
pQList->ErrorCode = HAL_DMA_QUEUE_ERROR_BUSY;
return HAL_ERROR;
}Seems like the DMA is busy.
I guess the Linked List is not well configured?
2025-03-04 1:12 AM
Hello,
did you receive my answer??
Not sure if i replied correctly ...
2025-03-04 5:56 AM
I did. I don't think you answered my second question.