2019-12-09 2:51 AM
Hello,
I don't understand the description of the Clock Security System in the Ref Manual of STM32H7 (section 7.5.3).
First question is : what exactly is the CSS doing ? (what kind of control is done on the clock). What is a definition of "a failure of the HSE" ?
Second question: the ref manual mentions both a dedicated interrupt rcc_hsecss_it and the NMI. Why is there both ? Why not only the NMI or only the interrupt ?
Thank you
Solved! Go to Solution.
2019-12-09 3:05 PM
When HSE stops ticking (due to xtal failure, PCB crack, short circuit or other), after some timeout the CSS (it's a slow-running resettable oscillator) triggers recovery actions to prevent complete clock loss. The rcc_hsecss_it is an internal signal of CSS and is connected to EXTI and NMI.
EXTI has one special feature - enables waking from STOP mode (of at least one CPU domain).
2019-12-09 3:05 PM
When HSE stops ticking (due to xtal failure, PCB crack, short circuit or other), after some timeout the CSS (it's a slow-running resettable oscillator) triggers recovery actions to prevent complete clock loss. The rcc_hsecss_it is an internal signal of CSS and is connected to EXTI and NMI.
EXTI has one special feature - enables waking from STOP mode (of at least one CPU domain).
2019-12-09 11:47 PM
Thank you Tomas, crystal clear. I would suggest to add these precisions in the ref manual.