2021-09-17 2:22 AM
Hi,
I want to use an STM32H743 for sampling one TIM.CNT and one ADC channel synchronously and store the data of both peripherals in array buf_adc[5000] and buf_timcnt[5000].
Therefore I want to use the DMAMUX request generation and use LPTIM2 as trigger with a update frequency of 6 MHz.
I configured two DMA channels in circular mode in CUBE and the LPTIM2 as request generator.
For testing I use one TIM.CNT and transfer the data from this register two both memory buffers to check for synchronous sampling.
I tested the DMA streams synchronous sampling by checking NDTR register for both streams. This value of NDTR is consistent, but if I compare the two arrays, one is showing a perfect sawtooth signal and the other one shows just trash.
Has anyone ever tried to synchonize two DMA transfers at this high frequency or/and can help me with this problem?
It seems the DMA transfer is corrupted.
2021-09-17 3:57 AM
Does it work at lower speeds?
If that fails then clearly that's a red herring..
2021-09-17 4:14 AM
2021-09-17 4:19 AM
I will check again if the serial connection, where is send data to the pc is fine. Maybe that's a problem
2021-09-17 4:38 AM
Serial connection is fine. It really seems to be a DMA problem.
2021-09-24 3:00 AM
Hi @DFlad.1 ,
Is your application based on a code generated with latest versions of STM32CubeMX (6.3.0) or STM32CubeIDE (1.7.0)?
If yes, please make sure that MX_DMA_Init() is called before peripheral initialization.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.