2023-06-06 3:28 AM
RM0444 rev. 5, sec. 29.3.4 and RM0490 rev. 3, sec. 21.3.4 both employ only WDGTB[1:0], but WWDG_CFR description mentions WDGTB[2:0] with eight different prescaler settings. So actually two or three bits?
Solved! Go to Solution.
2023-06-06 3:51 AM
Thank you for bringing this to our attention!
That indeed looks like a copy'n'paste typo. In fact, the time base of the WWDG has been extended compared to previous implementations and has three bits. The text strings WDGTB[1:0] still to be found in these RM should therefore be read as WDGTB[2:0].
Regards
/Peter
@Imen DAHMEN
2023-06-06 3:51 AM
Thank you for bringing this to our attention!
That indeed looks like a copy'n'paste typo. In fact, the time base of the WWDG has been extended compared to previous implementations and has three bits. The text strings WDGTB[1:0] still to be found in these RM should therefore be read as WDGTB[2:0].
Regards
/Peter
@Imen DAHMEN
2023-06-06 6:26 AM
Hello All,
Thank you for rising this up.
Internal ticket (ID 154205) is submitted to correct the typos in RM0444 and RM0490.
(PS: ID 154205 is an internal tracking number and is not accessible or usable by customers).
Imen