2023-11-21 1:45 AM - last edited on 2023-11-23 5:14 AM by PatrickF
Hello,
I would like to know if there are people who have already configured the SAI with a CODEC to recover the data ? With this link below:
https://wiki.st.com/stm32mpu/wiki/SAI_device_tree_configuration
I can see this figure but I don't quite understand this configuration. I know a little about SAI but not in depth.
I don't understand the line SDA from the SAI to the CODEC, what is this line for ?
Thank you for your helps.
Regards
2023-11-21 7:47 AM
HI @DYann.1
have you looked at https://wiki.st.com/stm32mpu/wiki/Soundcard_configuration#STM32MP15_disco_board_sound_card_configuration ?
Regards.
2023-11-23 2:40 AM
Hi,
I looked at your link there is this part that interests me but it is not the same microprocessor.
I don't have a STM32MP15 disco board, I have STM32L552ZET6QU microcontroller. Your link is too general and does not explain how to configure the SAI simply without having to read tons of pages to know how to do anything afterwards. Simpler and more practical please.
Thank you
2023-11-23 5:13 AM
Hi @DYann.1 ,
you originally posted this ticket in MPU forum.
STM32MP1 products are running Linux. For sure very different than STM32L5 way of working.
moved in right location,
regards.
2023-11-23 5:57 AM - edited 2023-11-23 5:59 AM
Hi,
You can see :
The SAI is inside the MCU inside the microprocessor to my knowledge right ? Where did you see it in linux for my Topic ?
Where should I put this topic? Can you move it to the correct section ?
Thank you
2023-11-23 6:25 AM
Hi,
I already moved on 'MCU topic' on purpose, which was created on
and you mention a wiki MPU link related to device tree (which is a Linux concept) in your initial post.
Don't worry, it is easy to mix-up, and we are here to help you.
For MCU, maybe have a look to https://www.st.com/content/st_com/en/stm32-mcu-developer-zone.html
Regards.
2023-11-23 6:35 AM
Thank you for this move to the correct section. But Now my question is much simpler than you think. We talk a lot to say nothing. Look at my question at the very beginning of the topic.
For this question I you gave me links and I wasted an entire day reading your documentation which is of absolutely no use. The document is very complete, even too complete, there is everything except the solution! Maybe it's your job to drown people like me in documentation ?
2023-11-23 9:05 AM
Sorry, I don't work on MCU products, but I can try to answer for HW point of view.
FS is synchro (usually audio sample rate)
SCK is clock for serial data sent on SDA and receive on SDB (if there is audio input path). usually 256xFS
info in STM32L5-Peripheral_Serial_Audio_Interface_SAI.pdf
Regards
2023-11-23 1:11 PM
Hi,
Thank you, we are approaching the subject (after your .pdf) this information is interesting :
After your explanation you say : 'SCK is clock for serial data sent on SDA and receive on SDB (if there is audio input path)'
But I have nothing to send, I just need to retrieve the values sent by the CODEC via the SAI only, in this case I just use the SDB right ,
Currently I have this configuration :
And it works, I can simulate data sent by the CODEC with an array initialized by myself and I receive the values in the RX array. Now I move on to another step which consists of recovering the real data sent by the CODEC. In this case I don't needto use SD_B right ?
Probably, I keep this configuration but in my code I will only use SD_A (which I use to retrieve the data).