2025-01-23 1:51 AM
I'm using STM32G030F6 chip. Try configure on pin PA8 external interrupt. When it make in UI "PInout & Configuration" tab it works as expected. But I want configure it from code. Here example:
Added to main.h pin naming
#define FC_ON_Pin GPIO_PIN_8
#define FC_ON_GPIO_Port GPIOA
#define FC_ON_EXTI_IRQn EXTI4_15_IRQn
function for pin setup
void FlyControler_Init(void){
#ifdef FC_PINIO
GPIO_InitTypeDef GPIO_InitStruct = {0};
/*Configure GPIO pins : FC_ON_Pin */
GPIO_InitStruct.Pin = FC_ON_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(FC_ON_GPIO_Port, &GPIO_InitStruct);
#endif
}
After call this function interrupt is not triggered.
What I do wrong?
Solved! Go to Solution.
2025-01-23 2:17 AM
Fixed:
void EXTI4_15_IRQHandler(void)
{
/* USER CODE BEGIN EXTI4_15_IRQn 0 */
/* USER CODE END EXTI4_15_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(POWER_Pin);
/* USER CODE BEGIN EXTI4_15_IRQn 1 */
#ifdef FC_PINIO
HAL_GPIO_EXTI_IRQHandler(FC_ON_Pin);
#endif
/* USER CODE END EXTI4_15_IRQn 1 */
}Thanks!
2025-01-23 1:57 AM - edited 2025-01-23 1:58 AM
Compare carefully to the generated code. The is a _it.c file implementing the raw interrupt handlers and dispatching the corresponding HAL function that will finally call the HAL callback.
hth
KnarfB
2025-01-23 2:17 AM
Fixed:
void EXTI4_15_IRQHandler(void)
{
/* USER CODE BEGIN EXTI4_15_IRQn 0 */
/* USER CODE END EXTI4_15_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(POWER_Pin);
/* USER CODE BEGIN EXTI4_15_IRQn 1 */
#ifdef FC_PINIO
HAL_GPIO_EXTI_IRQHandler(FC_ON_Pin);
#endif
/* USER CODE END EXTI4_15_IRQn 1 */
}Thanks!