cancel
Showing results for 
Search instead for 
Did you mean: 

Help in finding a ADC with 10K SPS < Sampling rate > 3K SPS and with 20 < resolution > 14 bits

umair_ejaz04
Associate II

Hello everyone,

I'm currently in search of an Analog-to-Digital Converter (ADC) for a project I'm working on and would greatly appreciate your recommendations. Here are the specific requirements:

  • Sampling Rate: Between 10 Samples Per Second (SPS) and 3,000 Samples Per Second (SPS)
  • Resolution: Between 14 bits and 20 bits
  • Compatibility: Will be using it with an STM32 Nucleo H743ZI2

If anyone has experience with ADCs that fit these criteria or can suggest reliable models, please share your insights. Additionally, any advice on suppliers or vendors who offer good deals on such components would be very helpful.

Thank you in advance for your assistance!

5 REPLIES 5
AScha.3
Chief II

Hi,

so why not using the one of the ADCs in H743 ?

AScha3_0-1720805685026.png

 

 

They easily fulfill your requirements .

If you feel a post has answered your question, please click "Accept as Solution".
TDK
Guru

Your requirements aren't particularly hard to meet. There are parametric searches at most suppliers with thousands of results for those. Use one with an SPI interface for easy interface to the chip.

> vendors who offer good deals on such components

If budget is a concern, using the built-in 16-bit ADC on the STM32H7 (16 bit) seems a better choice. Note that the analog design needs to be done well in order to get suitable precision from the ADC. If you want 14 bits of precision, you'll need to incorporate many of the design suggestions here:

cd00211314-how-to-get-the-best-adc-accuracy-in-stm32-microcontrollers-stmicroelectronics.pdf

If you feel a post has answered your question, please click "Accept as Solution".

I have to use 5 ADC's.

budget is not a concern.

H743 has up to 20 ADC inputs.

If you feel a post has answered your question, please click "Accept as Solution".