cancel
Showing results for 
Search instead for 
Did you mean: 

Documentation: USART1/2 and APB2/1 on STM32U5 series

FB1
Associate II

Is USART1 on APB1 (AN5593, tab.17) or APB2 (DS, RM, CubeMX) and USART2 on APB1 (DS, RM, CubeMX) or APB2 (AN5593, tab.17)? Guess, there is an issue in an5593-how-to-use-the-gpdma-for-stm32u5-series-microcontrollers-stmicroelectronics Rv.4 , isn‘t it?

1 ACCEPTED SOLUTION

Accepted Solutions
Sarra.S
ST Employee

Hello @FB1

As @TDK already said, the RM and DS are correct. 

I reported the AN5593 documentation issue to be corrected (Internal ticket number 165109)  

Thank you! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
TDK
Guru

The RM/DS is correct.

When in doubt, you can go into the code and look at the memory address of USART1 and USART2 to see which one they're in.

TDK_0-1698418353197.png

 

If you feel a post has answered your question, please click "Accept as Solution".
Sarra.S
ST Employee

Hello @FB1

As @TDK already said, the RM and DS are correct. 

I reported the AN5593 documentation issue to be corrected (Internal ticket number 165109)  

Thank you! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.