2025-02-18 5:15 AM
Good afternoon,
I am currently trying to calibrate my ADC4 of my NUCLEO U545 and I am using the following function:
HAL_ADCEx_Calibration_Start(&hadc4, CalibrationMode, SingleDiff);As said before the first parameter is going to be the ADC4 that I am using but what about the other two parameters?
What are they exactly? Do i have to declare the parameters somewhere in the code? Is there anyway that I can see in the documentation what are this parameters and the value i have to introduce to them? And finally, the ADC1 configuration is done the same way as in the ADC4?
Thank you,
Marc
Solved! Go to Solution.
2025-02-18 5:38 AM
The source code is documented and shows what the arguments should be. In this case:
/**
* @brief Perform an ADC automatic self-calibration
* Calibration prerequisite: ADC must be disabled (execute this
* function before HAL_ADC_Start() or after HAL_ADC_Stop() ).
* @PAram hadc ADC handle
* @PAram CalibrationMode Selection of calibration offset or
* linear calibration offset.
* @arg ADC_CALIB_OFFSET Channel in mode calibration offset
* @arg ADC_CALIB_OFFSET_LINEARITY Channel in mode linear calibration offset
* @PAram SingleDiff Selection of single-ended or differential input
* This parameter can be one of the following values:
* @arg @ref ADC_SINGLE_ENDED Channel in mode input single ended
* @arg @ref ADC_DIFFERENTIAL_ENDED Channel in mode input differential ended
* @retval HAL status
*/
HAL_StatusTypeDef HAL_ADCEx_Calibration_Start(ADC_HandleTypeDef *hadc, uint32_t CalibrationMode, uint32_t SingleDiff)
Probably you want this:
HAL_ADCEx_Calibration_Start(&hadc4, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
Further information on these can be found in the reference manual in the section "33.4.8 Calibration (ADCAL, ADCALLIN, ADC_CALFACT)".
> And finally, the ADC1 configuration is done the same way as in the ADC4?
Yes.
2025-02-18 5:38 AM
The source code is documented and shows what the arguments should be. In this case:
/**
* @brief Perform an ADC automatic self-calibration
* Calibration prerequisite: ADC must be disabled (execute this
* function before HAL_ADC_Start() or after HAL_ADC_Stop() ).
* @PAram hadc ADC handle
* @PAram CalibrationMode Selection of calibration offset or
* linear calibration offset.
* @arg ADC_CALIB_OFFSET Channel in mode calibration offset
* @arg ADC_CALIB_OFFSET_LINEARITY Channel in mode linear calibration offset
* @PAram SingleDiff Selection of single-ended or differential input
* This parameter can be one of the following values:
* @arg @ref ADC_SINGLE_ENDED Channel in mode input single ended
* @arg @ref ADC_DIFFERENTIAL_ENDED Channel in mode input differential ended
* @retval HAL status
*/
HAL_StatusTypeDef HAL_ADCEx_Calibration_Start(ADC_HandleTypeDef *hadc, uint32_t CalibrationMode, uint32_t SingleDiff)
Probably you want this:
HAL_ADCEx_Calibration_Start(&hadc4, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
Further information on these can be found in the reference manual in the section "33.4.8 Calibration (ADCAL, ADCALLIN, ADC_CALFACT)".
> And finally, the ADC1 configuration is done the same way as in the ADC4?
Yes.