2023-05-23 05:47 AM
Hi,
I am trying to communicate with i2c DMA without interrupt. My MCU is STM32G474RET6.
I've read that it is possible but can't find how to do it.
How can i communicate in slave mode with i2c dma?
Since my interrupts disabled, can't use the callback functions. I've checked the signal and after address, bus is hanged and not gave ACK.
2023-05-23 07:02 AM - edited 2023-11-20 04:47 AM
Hello @Günce Yasan ,
For I2C communication using DMA, you should configure DMA setting using STM32CubeMX by adding I2Cx_TX or I2Cx_RX as showing in the figure :
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-23 07:07 AM - edited 2023-11-20 04:48 AM
Hi @KHALSI_Foued
Yes i did those configurations. Here's my cubemx conf. Normally when interrupt enabled, i use callback functions to do my receive/transmit proccess. Since i don't use interrupt, i see in my function I2C ADDR flag is set, and after that i try to receive with dma but my program goes into infinite loop. Is there some function i should call before receive func. or etc. ?
2023-05-23 07:13 AM
Open main.c
add :
/* Receive in master mode an amount of data in non-blocking mode with DMA */
HAL_I2C_Master_Receive_DMA(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint8_t *pData,uint16_t Size)
and try to put this function between user code begin 4 and user code end 4 to make sure that the transfer completed :
/*Master Rx Transfer completed callback. */
void HAL_I2C_MasterRxCpltCallback(I2C_HandleTypeDef *I2cHandle)
{
/* ########### */
}
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-23 10:43 PM - edited 2023-11-20 04:48 AM
I am working in slave mode so i used slave configurations. Here is my code.
The LED is toggling. But it doesn't goes into the callback.
I see from my ISR reg the address is matched. But after that can't take the command.
2023-06-05 11:17 AM
Hi @Günce Yasan
The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.
Regards,
Billy
2024-03-30 02:12 AM
hi @gunccc
have you got any solution for this problem?
because im also facing same issue... when im calling HAL_I2C_Mem_Write_DMA function then salve is going into BUSY state and after that not comint out from BUSY state at all. but HAL_I2C_Mem_Write is working fine.