cancel
Showing results for 
Search instead for 
Did you mean: 

Generate PWM output based on input capture

VGani.1
Associate III

Hi, 

I am trying to sense a signal through TIM1 channel 1 by configuring as Input capture and Measure the signal frequency and Pulse width. Now I want to generate a signal with a phase delay after the falling edge of the input capture pulse. It should turn ON after the falling edge with some delay and turn OFF after triggering next rising edge. How to configure the channel? can we use other channel in the same timer?? or need to select other Timer for generating Signal??

 

Regards

Vijay

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0