cancel
Showing results for 
Search instead for 
Did you mean: 

CAN1 RX issue

Ash1
Associate III

Hi

I am using STM32F407 evb in which I have configured both CAN1 and CAN2 ,I am sendind CAN1(3 ids 501,502,503) and vice versa from CAN2 same I am sending but I am ble to recive all three id on CAN2 Rx but only one ID iam receving on CAN1(501) .I am sahring my filter configuration I am using mask mode 

 

if (can_controller==0){

		for (int i=0; i <CAN_MAXTABLEID_0; i++)
		{
			Can_Configfilter[i].FilterIdHigh = (0x501 << 5);
			Can_Configfilter[i].FilterMaskIdHigh =(0xFFC << 5);
			Can_Configfilter[i].FilterIdLow = 0x00000000;      // Initialize if EXTID used
			Can_Configfilter[i].FilterMaskIdLow = 0x00000000;  //  Initialize if EXTID used
			Can_Configfilter[i].FilterFIFOAssignment = CAN_FILTER_FIFO_0;
			Can_Configfilter[i].FilterBank = i;                //Selection of filterBANk
			Can_Configfilter[i].FilterMode = CAN_FILTERMODE_IDMASK;  // Identifier mode
			Can_Configfilter[i].FilterScale = CAN_FILTERSCALE_32BIT;  // Scale selection
			Can_Configfilter[i].FilterActivation = CAN_FILTER_ENABLE;// Example activation
			Can_Configfilter[i].SlaveStartFilterBank=1;                //0-2 CAN1 filter

			Can_IPW_Can_ConfigFilter(&hcan,&Can_Configfilter[i]);  //Filter configuration
		}
}


	if (can_controller==1){

			for (int i=1; i <CAN2_MAXTFILTER; i++)
			{
				Can_Configfilter[i].FilterIdHigh = (0x501 << 5);
				Can_Configfilter[i].FilterMaskIdHigh =( 0xFFC << 5);
				Can_Configfilter[i].FilterIdLow = 0x00000000;      // Initialize if EXTID used
				Can_Configfilter[i].FilterMaskIdLow = 0x00000000;  //  Initialize if EXTID used
				Can_Configfilter[i].FilterFIFOAssignment = CAN_FILTER_FIFO_0;
				Can_Configfilter[i].FilterBank = i;                //Selection of filterBANk
				Can_Configfilter[i].FilterMode = CAN_FILTERMODE_IDMASK;  // Identifier mode
				Can_Configfilter[i].FilterScale = CAN_FILTERSCALE_32BIT;  // Scale selection
				Can_Configfilter[i].FilterActivation = CAN_FILTER_ENABLE;// Example activation
				Can_Configfilter[i].SlaveStartFilterBank=1;                //2-28 CAN2 filter

				Can_IPW_Can_ConfigFilter(&hcan,&Can_Configfilter[i]);  //Filter configuration
			}
	}

 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

I've created a simple project where CAN1 and CAN2 are in loopback mode using STM32F407 Discovery board and I'm receiving well all the sent IDs: 0x502 (1281), 0x502 (1282), 0x503 (1283) on both sides CAN1 and CAN2:

CAN1 Rx:

SofLit_0-1735914523248.png

CAN2 Rx:

SofLit_1-1735914574561.png

I've attached the project.

I've also used that configuration and worked fine:

 

  sFilterConfig.FilterBank = 0;
  sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
  sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
  sFilterConfig.FilterIdHigh = (0x501 << 5);
  sFilterConfig.FilterIdLow = 0x0000;
  sFilterConfig.FilterMaskIdHigh = (0xFFC << 5);
  sFilterConfig.FilterMaskIdLow = 0x0000;
  sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
  sFilterConfig.FilterActivation = ENABLE;
  sFilterConfig.SlaveStartFilterBank = 1;
  
  if(HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
  {
    /* Filter configuration Error */
    Error_Handler();
  }
  
  sFilterConfig.FilterBank = 1;
  sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
  sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
  sFilterConfig.FilterIdHigh = (0x501 << 5);
  sFilterConfig.FilterIdLow = 0x0000;
  sFilterConfig.FilterMaskIdHigh = (0xFFC << 5);
  sFilterConfig.FilterMaskIdLow = 0x0000;
  sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
  sFilterConfig.FilterActivation = ENABLE;
  sFilterConfig.SlaveStartFilterBank = 1;
  
  if(HAL_CAN_ConfigFilter(&hcan2, &sFilterConfig) != HAL_OK)
  {
    /* Filter configuration Error */
    Error_Handler();
  } 

 

So I suspect something wrong in your specific implementation, either in your Can_IPW_Can_ConfigFilter() or with the handler hcan that was not set correctly in your software.

Hope it helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

21 REPLIES 21
SofLit
ST Employee

Hello,

For "controller 1" (I think CAN1). Here i starts from 0:

for (int i=0; i <CAN_MAXTABLEID_0; i++)

For "controller 2" (I think CAN2). Here i starts from 1:

for (int i=1; i <CAN2_MAXTFILTER; i++)

So what are the values of CAN_MAXTABLEID_0 and CAN2_MAXTFILTER?

I suspect an overlap of Filter config between CAN1 and CAN2!  -> CAN_MAXTABLEID_0 should not exceed 1

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Ash1
Associate III

hi  

value as follows 

CAN_MAXTABLEID_0 =1, and CAN2_MAXTFILTER=2

1. I Think filter configuration is fine .

First I am sending 3 id from CAN1 then 3 id From CAN2 in this case CAn2 is receving all three but CAn1 only one id.

2.than I interchange sending way this time I sent CAN2 first and CAN1 after ,in this case CAN2 receving only one and CAN1 receving all three IDs,

I am sending in 10 ms function.

For the moment use "pass all" IDs filters for CAN1:

Can_Configfilter[i].FilterIdHigh = 0x0000;
Can_Configfilter[i].FilterMaskIdHigh = 0x0000;
Can_Configfilter[i].FilterIdLow = 0x0000;      
Can_Configfilter[i].FilterMaskIdLow = 0x0000; 

And see if you get all the messages intended to be received.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Ash1
Associate III

Hi

I have tried as u said still CAN1 only one ID I am receiving even CAN1 tx buffer and CAn2 tx buffer value is filled with correct DATA. in my CAN1 inside RF0R -> FMP value is only going upto one . and in CAN2 FMP value is getting upto 3.

NOTE: with the same I used to transmit from CAN2 to CAN1 it is working fine but when I m using both CAN1 and CAN2 at one time I am facing issue.

Also you used the same handle for both controller "hcan" to set the filters:

Can_IPW_Can_ConfigFilter(&hcan,&Can_Configfilter[i]);

Also Can_IPW_Can_ConfigFilter() is not part of HAL. It's your implementation. Also I don't see why you repeat the same filter config for CAN2 (two iterations for the same config!).

So at this stage, I suggest you to go step by step and start by using a very simple example:

if (can_controller==0)
{
  sFilterConfig.FilterBank = 0;
  sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
  sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
  sFilterConfig.FilterIdHigh = 0x0000;
  sFilterConfig.FilterIdLow = 0x0000;
  sFilterConfig.FilterMaskIdHigh = 0x0000;
  sFilterConfig.FilterMaskIdLow = 0x0000;
  sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
  sFilterConfig.FilterActivation = ENABLE;
  sFilterConfig.SlaveStartFilterBank = 1;
  HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig)
}


if (can_controller==1)
{
  sFilterConfig.FilterBank = 1;
  sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
  sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
  sFilterConfig.FilterIdHigh = 0x0000;
  sFilterConfig.FilterIdLow = 0x0000;
  sFilterConfig.FilterMaskIdHigh = 0x0000;
  sFilterConfig.FilterMaskIdLow = 0x0000;
  sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
  sFilterConfig.FilterActivation = ENABLE;
  sFilterConfig.SlaveStartFilterBank = 1;
 HAL_CAN_ConfigFilter(&hcan2, &sFilterConfig)
}

 Here CAN1 and CAN2 are separated. If this works please add your Mask id config and try .. and so on.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Ash1
Associate III

hi

Yes this is my code Hcan I am just using to check the state only nothing else.

apart from this one more query i wanted to run only can2Tx and CAn1 RX so I am sending 6 ID from CAN2 even I disable fifolocked but I am able to recive only 3 id .other three I am not reciving . CAN1 filter I configured for 0x0000 and MAsk too.  

whatever three id I am sending first only those id I am ble to recivie so Why I am lossing other ID?anyIDEA

As said previously, I suggest to go step by step and start by using simple examples and debug.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Ash1
Associate III

Hi 

I have tried the same still CAN1 RX(one id) issue CAN2 is fine(all three ID)

if (can_controller==0){
		CAN_FilterTypeDef sFilterConfig;
		  sFilterConfig.FilterBank = 0;
		  sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
		  sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
		  sFilterConfig.FilterIdHigh = 0x0000;
		  sFilterConfig.FilterIdLow = 0x0000;
		  sFilterConfig.FilterMaskIdHigh = 0x0000;
		  sFilterConfig.FilterMaskIdLow = 0x0000;
		  sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
		  sFilterConfig.FilterActivation = ENABLE;
		  sFilterConfig.SlaveStartFilterBank = 1;
		  Can_IPW_Can_ConfigFilter(&hcan, &sFilterConfig);

}


	if (can_controller==1){
		CAN_FilterTypeDef sFilterConfig1;
		sFilterConfig1.FilterBank = 1;
		sFilterConfig1.FilterMode = CAN_FILTERMODE_IDMASK;
		sFilterConfig1.FilterScale = CAN_FILTERSCALE_32BIT;
		sFilterConfig1.FilterIdHigh = 0x0000;
		sFilterConfig1.FilterIdLow = 0x0000;
		sFilterConfig1.FilterMaskIdHigh = 0x0000;
		sFilterConfig1.FilterMaskIdLow = 0x0000;
		sFilterConfig1.FilterFIFOAssignment = CAN_RX_FIFO0;
		sFilterConfig1.FilterActivation = ENABLE;
		sFilterConfig1.SlaveStartFilterBank = 1;
		Can_IPW_Can_ConfigFilter(&hcan, &sFilterConfig1);

st 

This is not the code I shared to test from your side:


@Ash1 wrote:
if (can_controller==0){
		CAN_FilterTypeDef sFilterConfig;
		  sFilterConfig.FilterBank = 0;
		  sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
		  sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
		  sFilterConfig.FilterIdHigh = 0x0000;
		  sFilterConfig.FilterIdLow = 0x0000;
		  sFilterConfig.FilterMaskIdHigh = 0x0000;
		  sFilterConfig.FilterMaskIdLow = 0x0000;
		  sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
		  sFilterConfig.FilterActivation = ENABLE;
		  sFilterConfig.SlaveStartFilterBank = 1;
		  Can_IPW_Can_ConfigFilter(&hcan, &sFilterConfig);

}


	if (can_controller==1){
		CAN_FilterTypeDef sFilterConfig1;
		sFilterConfig1.FilterBank = 1;
		sFilterConfig1.FilterMode = CAN_FILTERMODE_IDMASK;
		sFilterConfig1.FilterScale = CAN_FILTERSCALE_32BIT;
		sFilterConfig1.FilterIdHigh = 0x0000;
		sFilterConfig1.FilterIdLow = 0x0000;
		sFilterConfig1.FilterMaskIdHigh = 0x0000;
		sFilterConfig1.FilterMaskIdLow = 0x0000;
		sFilterConfig1.FilterFIFOAssignment = CAN_RX_FIFO0;
		sFilterConfig1.FilterActivation = ENABLE;
		sFilterConfig1.SlaveStartFilterBank = 1;
		Can_IPW_Can_ConfigFilter(&hcan, &sFilterConfig1);

Please use the code I shared above. As I said Can_IPW_Can_ConfigFilter() is not part of the HAL and it's your implementation and hcan handle usage still ambiguous. So at this stage please use HAL_CAN_ConfigFilter() instead:

 

if (can_controller==0)
{
  sFilterConfig.FilterBank = 0;
  sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
  sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
  sFilterConfig.FilterIdHigh = 0x0000;
  sFilterConfig.FilterIdLow = 0x0000;
  sFilterConfig.FilterMaskIdHigh = 0x0000;
  sFilterConfig.FilterMaskIdLow = 0x0000;
  sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
  sFilterConfig.FilterActivation = ENABLE;
  sFilterConfig.SlaveStartFilterBank = 1;
  HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig)
}


if (can_controller==1)
{
  sFilterConfig.FilterBank = 1;
  sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
  sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
  sFilterConfig.FilterIdHigh = 0x0000;
  sFilterConfig.FilterIdLow = 0x0000;
  sFilterConfig.FilterMaskIdHigh = 0x0000;
  sFilterConfig.FilterMaskIdLow = 0x0000;
  sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
  sFilterConfig.FilterActivation = ENABLE;
  sFilterConfig.SlaveStartFilterBank = 1;
 HAL_CAN_ConfigFilter(&hcan2, &sFilterConfig)
}

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.