2025-02-05 12:49 AM - last edited on 2025-02-05 01:01 AM by Andrew Neil
Hi
Can you tell me how I can calculate a value for ARR for timer 2(32bit timer) and timer3(16bit timer)
I am using STM32F407 APB1 timer clock is 12MHz prescaler is 6
2025-02-05 02:44 AM - edited 2025-02-05 03:34 AM
Timer settings seems to be right. Have you done clock configuration in CubeMX? Please check if time clock (APB1 Timer clocks) is really 72 MHz.
Set CKD in (TIMx_CR1) as 00 should be correct
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-05 02:54 AM
2025-02-05 03:00 AM
Sounds like you're clocking at 100 or 108 MHz, not 72
Check your PLL and HSE relationships
2025-02-05 03:34 AM
hi
Can you suggest me a code in which there is generated interrupt using any timer
2025-02-05 03:38 AM - edited 2025-02-05 03:41 AM
@Ash1 wrote:
hi
Can you suggest me a code in which there is generated interrupt using any timer
Time base with interrupt:
PS: No ioc file available for this example.
2025-02-05 03:48 AM - edited 2025-02-05 03:48 AM
@Ash1 wrote:Can you suggest me a code in which there is generated interrupt using any timer
The code posted by @SofLit in the very first reply !
2025-02-05 04:57 AM - edited 2025-02-05 05:27 AM
Hi
I have recheked my configuration and found it was 84mhz timer clock instead of 72Mhz
so for 10 second I am loading 0x98967F in ARR and 83 i have loaded in PSC register but still timer is generating UIF flag sometimes in 7 seconds 4 seconds 2 seconds .can you help me Why I am facing this irregular intervals of setting UIF flag
Note :Do i have to set URS bit also in CR1 will it effec