2024-10-22 11:58 PM - last edited on 2024-10-23 04:36 AM by mƎALLEm
void SystemClock_Config(void)
{
// Step 1: Enable HSI
RCC->CR |= RCC_CR_HSION; // Enable HSI
while (!(RCC->CR & RCC_CR_HSIRDY)); // Wait until HSI is ready
// Step 2: Configure the voltage scaling
PWR->CR1 |= PWR_CR1_VOS_0; // Set voltage scale to 1 (VOS = 1)
// Step 3: Configure the PLL
RCC->PLLCFGR = 0; // Clear PLL configuration register
RCC->PLLCFGR |= (1 << RCC_PLLCFGR_PLLM_Pos) | // PLLM = 1
(10 << RCC_PLLCFGR_PLLN_Pos) | // PLLN = 10 (HSI frequency * 10 = 80 MHz)
(0 << RCC_PLLCFGR_PLLP_Pos) | // PLLP = 2 (DIV2)
(2 << RCC_PLLCFGR_PLLQ_Pos) | // PLLQ = 2 (DIV2)
(2 << RCC_PLLCFGR_PLLR_Pos) | // PLLR = 2 (DIV2)
RCC_PLLCFGR_PLLSRC_HSI; // PLL source = HSI
// Step 4: Enable the PLL
RCC->CR |= RCC_CR_PLLON; // Enable PLL
while (!(RCC->CR & RCC_CR_PLLRDY)); // Wait until PLL is ready
// Step 5: Set PLL as the system clock source
RCC->CFGR &= ~RCC_CFGR_SW; // Clear SW bits
RCC->CFGR |= RCC_CFGR_SW_PLL; // Set PLL as the system clock source
while ((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_PLL); // Wait until PLL is used as system clock
// Step 6: Configure the AHB and APB prescalers
RCC->CFGR &= ~RCC_CFGR_HPRE; // AHB prescaler = 1
RCC->CFGR &= ~RCC_CFGR_PPRE1; // APB1 prescaler = 1
RCC->CFGR &= ~RCC_CFGR_PPRE2; // APB2 prescaler = 1
// Step 7: Configure flash latency
FLASH->ACR &= ~FLASH_ACR_LATENCY; // Clear latency bits
FLASH->ACR |= FLASH_ACR_LATENCY_4WS; // Set latency to 4 wait states for 80 MHz
}
The code doesn't break out of while loop.
I am struck in the step 5. unable to resolve the issue.
// Step 5: Set PLL as the system clock source. Help me resolve this issue.
2024-10-23 12:10 AM
You have to set APB prescalers, and, more importantly, the FLASH waitstates, *before* you switch the system clock to PLL in RCC_CFGR.
JW
2024-10-23 01:10 AM
PWR must be enabled in RCC before use.
2024-10-23 01:32 AM
> PWR must be enabled in RCC before use.
Correct; however, Range 1 is the default VOS setting anyway.
JW
2024-10-23 02:14 AM
Also, the value written to PLLM, PLLP, PLLQ and PLLR fields is the divisor value - 1.
You may find the working clock setup code in my USB stuff, link in signature - Example/Inc/L4 folder.
2024-10-23 04:32 AM - edited 2024-10-23 04:33 AM
In the mid-range 'L4, the Q and R dividers are 2 * (value + 1), and P is quite bizarre, 7 or 17... and HSI frequency is 16MHz. These things tend to change from STM32 to STM32 (sub)family.
> link in signature
I don't see any signature in this thread (https://community.st.com/t5/stm32-mcus-products/bare-metal-stm32l496/m-p/734800 ).
JW
2024-10-23 04:38 AM
Hello @vbk22398 ,
In next time please use </> button to post your code. See these tips on posting a thread.
Thank you for your understanding.
2024-10-23 05:05 AM
2024-10-23 06:04 AM
Interesting. I don't see it.
But by this point I gave up any attempts to comment on the state of affairs; it's just waste of time and energy. I have better places to be ignored.
JW
2024-11-12 10:50 AM - edited 2024-11-12 10:52 AM
I was wrong about the signature, and it's my fault.
I've been approached by an Admin who told me, that I have switched off displaying signatures in my settings - which I indeed have done back then when Khoros was new, in order to decrease visual noise and try to squeeze in as much relevant information on a screenful as possible - and have forgotten about it since then.
(And I've been also confused by the fact that I do see signatures, when I am not logged in.)
JW