2024-11-08 8:39 PM
....so says STM32F334x4/x6/x8 Errata sheet STM32F334x4/x6/x8 Rev Z device limitations
Doc is dated 2021. No answers seen on web.
Has this been fixed yet?
If not, will it be fixed? And if so, when?
Ta lots
Rex
2024-11-11 2:45 AM
Hello @RexG
unfortunately, there is not any available workaround for now and there is not any potential solution on going. For the typo on table 4 where it is mentioned that there is an existing workaround. It is just a typo on the errata sheet that I've escalated for correction on the coming release (under internal ticket number 196061).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-12 12:14 PM
That's a very simple mask fix!
Badly done ST!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.