cancel
Showing results for 
Search instead for 
Did you mean: 

Alarm waking up befor 1 Min when after 2 or 3 days

Kai_Satone
Associate III

i am using stm32f41ceu6 with RTC and RCC in that we are using LSE  with 100HZ 
if i set  Alarm  for 1H or more then still working but after 2 or 3 days it wakeup early befor one Min
example i set alarm at 11:30 then it will wakeup after one hour that time after 2 or 3 days wakeup day 11:29
there need of any other calibration or any other solution 
 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

You need to calibrate the RTC. Review this article.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
mƎALLEm
ST Employee

Hello,

You need to calibrate the RTC. Review this article.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

thank you sir