cancel
Showing results for 
Search instead for 
Did you mean: 

AD5668 DAC over QSPI on STM32L4

Gowthami412
Associate II

New question from: https://community.st.com/t5/stm32-mcus-products/qspi-master-and-slave/td-p/758418

I have a AD5668 DAC which supports QSPI upto 50Mhz frequency. I am trying to test the DAC with STM32 using QSPI . But I am not able to see DAC output. So I thought to debug it with two Microcontrollers like how we do with SPI. 

This is my code

// Function to send data to AD5668 DAC in the specified format

void AD5668_SendCommand(uint8_t command, uint8_t channel, uint16_t voltage) {

uint8_t commandData[4];

QSPI_CommandTypeDef sCommand = {0};

HAL_StatusTypeDef status;

// QSPI command configuration

sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;

sCommand.AddressMode = QSPI_ADDRESS_NONE;

sCommand.DataMode = QSPI_DATA_1_LINE;

sCommand.DummyCycles = 0;



commandData[0] = command; // Command byte (e.g., 0x03)

commandData[1] = channel; // Channel byte (e.g., 0x0F)

commandData[2] = (voltage >> ‌‌ & 0xFF; // MSB of voltage

commandData[3] = voltage & 0xFF; // LSB of voltage



// Transmit the command via QSPI

for(int i =0; i<4; i++)

{

status= HAL_QSPI_Transmit(&hqspi, &commandData[i], HAL_MAX_DELAY)!=HAL_OK;

HAL_Delay(10);

printf("status:%d\n",status);

}

int main(void)

{

AD5668_SendCommand(0x03, 0x1F, voltage); // Send command in the specified format

}



This is QSPI Initialization :

static void MX_QUADSPI_Init(void)

{

/* QUADSPI parameter configuration*/

hqspi.Instance = QUADSPI;

hqspi.Init.ClockPrescaler = 1;

hqspi.Init.FifoThreshold = 4;

hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;

hqspi.Init.FlashSize = 4;

hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_2_CYCLE;

hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;

hqspi.Init.FlashID = QSPI_FLASH_ID_1;

hqspi.Init.DualFlash = QSPI_DUALFLASH_DISABLE;

if (HAL_QSPI_Init(&hqspi) != HAL_OK)

{

Error_Handler();

}



}

Provide any suggestions why it is not working

 

3 REPLIES 3
filipxsikora
Associate III

First of all, you have configured your QSPI in 1 data line mode, which in turn makes it just a normal SPI. No point of using QSPI for this.

Quick glance through the Datasheet of the DAC shows, that the DAC does NOT support QSPI (well, okay, technically it does, but only in this one data line mode, which is effectively just normal SPI).

QSPI means QUAD-SPI -> that means 4 data lines in parallel + Clk -> that means 4x throughput per 1 clock cycle. And it makes sense to utilize that interface fully with appropriate peripherals, which actually support QSPI itf.

 

TL;DR: Just use normal SPI, save yourself the trouble.

KDJEM.1
ST Employee

Hello @Gowthami412 and welcome to the community;

 

For communication, the QUADSPI can only be used as master only, it cannot be a master and slave like SPI.

It is necessary to check the compatibility of the command between the QUADSPI interface and DAC device: such as command order (instruction phase, address phase, alternate-byte phase, dummy-cycle phase, data phase) and the bytes number for each command. 

For more information, look to Overall FAQs for QUADSPI/OCTOSPI/HSPI/XSPI and precisely "1.1. How to check whether a device is supported" and "1.5. Can I use the interfaces as classic-SPI?" FAQs 

May be these post can help you to use the QUADSPI interface as legacy SPI:

Solved: Can I use OCTOSPI as a Classic SPI? - STMicroelectronics Community

-  Solved: Which OCTOSPI pins can be used as MOSI and MISO in... - STMicroelectronics Community

Solved: Re: Octal SPI Interface - STMicroelectronics Community

 

I hope this help you.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you for your quick response. I will find an QSPI flash memory and will test QSPI using STM32.

 

Regards 

Gowthami412