2024-12-02 9:51 PM
I have tried connecting both STLink and UART but Motor Pilot is not getting connected,
ERROR: No STLink VCP detected
I am using (V1.2.9) and tried using older version but still issue persists. Kindly help.
2024-12-17 5:28 AM
Hello,
I think I found the issue, as you are using a non official STLink device, the Discover Board function will not work.
You need to load the GUI you need and then manually connect using the correct COM Port.
2024-12-17 7:33 PM
which GUI file should i load?
2025-01-14 11:58 AM
Hello,
i'm updated my sw from sdk 6.2 to 6.3 and now the Motor Pilot application does not work.
If i use the older version with simple USB to UART adapter it works fine.
Any suggestion? How to change the ST VCP settings to simple UART?
The communication menù still in grey color.
Windows 11, MC-SDK6.3.2, CUBE MX6.13.0, CUBE 17.0
Thanks, regards.
Giovanni