2024-12-02 09:51 PM
I have tried connecting both STLink and UART but Motor Pilot is not getting connected,
ERROR: No STLink VCP detected
I am using (V1.2.9) and tried using older version but still issue persists. Kindly help.
2024-12-17 05:28 AM
Hello,
I think I found the issue, as you are using a non official STLink device, the Discover Board function will not work.
You need to load the GUI you need and then manually connect using the correct COM Port.
2024-12-17 07:33 PM
which GUI file should i load?