2023-11-23 02:56 AM
Hello,
I put all values of pole pair speed current etc as show in below screenshot
but while during i start the profile speed feedback error i get
please let me know what is the problem
2023-11-23 03:14 AM
Did you check the hall sensor signals in the oscilloscope are they proper?
2023-11-23 03:16 AM
kindly please tell me how to check
2023-11-23 03:22 AM
Based on your hall sensor displacement you should be getting a waveform similar to above when the motor is running.
All the 3 hall sensor signals shall not be all low or high, then there is a problem. Tap the 3 hall sensor signals and check on oscilloscope.
2023-11-23 03:25 AM
how to connect u v w signals to oscilloscope
2023-11-23 03:26 AM
u v w means H1 H2 H3 for ref
2023-11-23 03:28 AM - edited 2023-11-23 03:31 AM
Do you use sensored (hall based) commutation?
H1,H2,H3 are hall signals
U,V,W are the inverter outputs. Both are different.
2023-11-23 03:32 AM
yes sir
2023-11-23 03:35 AM
i use sensored commutation