cancel
Showing results for 
Search instead for 
Did you mean: 

It is not clear where the value of SPEED_LOOP_FREQUENCY_HZ is defined.

AndrewSibiryack
Associate III

Hi!

Help!

When creating a position control project in the MC SDK using NUCLEO-F446RE and X-NUCLEO-IHM08M1-3Sh when compiling to KEIL, an error occurred.

It is not clear where the value of SPEED_LOOP_FREQUENCY_HZ is defined.

Thank you in advance!

1 ACCEPTED SOLUTION

Accepted Solutions
VFerr.2
Associate II

Replace by POSITION_LOOP_FREQUENCY_HZ in all files. It's a bug.

View solution in original post

4 REPLIES 4
VFerr.2
Associate II

Replace by POSITION_LOOP_FREQUENCY_HZ in all files. It's a bug.

AndrewSibiryack
Associate III

Thanks! Everything worked out!

Thanks @VFerr.2​ for sharing the solution.

@cedric H​ , could you please take care to implement the fix?

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @Amel NASRI​ 

This is a known issue already handled in the following thread

Regards

Cedric