Skip to main content
SVerm.6
Visitor II
April 12, 2022
Question

I am using STM32H743VITx controller and i want to interface it with a BLDC motor.

  • April 12, 2022
  • 0 replies
  • 626 views

While debugging the code everything works fine until i give command to start the motor i.e the moment i generate PWM and motor starts rotating, Cube IDE generates a message that the "target is not responding".

Also I've made sure that SWDIO, SWCLK, and SWO pins are correctly mapped on the controller.

This topic has been closed for replies.