2020-12-24 05:37 AM
2020-12-24 05:53 AM
Most things, less well, especially the debug.
2020-12-24 06:13 AM
Thank you for your quick reply and help.
2021-06-01 08:59 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
Laurent Ca...
2021-06-01 09:16 AM
They are all IDEs; they all do essentially the same stuff.
Keil & IAR are independent 3rd-party commercial closed-source IDEs.
2021-06-01 09:20 AM
>>Keil & IAR are independent 3rd-party commercial closed-source IDEs.
They are written and tested to far higher standards.
The optimizers work better and have less issues.
The debugging is better integrated and tends to "Just Work", rather than be a real dog's breakfast of poorly fitting parts.
2021-06-02 09:00 AM
and the price reflects this!