Skip to main content
Visitor II
February 6, 2025
Question

Freezing of the STM32CubeIDE environment when including a large file with a data array

  • February 6, 2025
  • 0 replies
  • 760 views

Hi.
I have a problem with CubeIDE. I need to attach a large sound file - 100k samples 8bit. After doing this, the environment stops working in a usable way. I keep getting messages:

 My hardware is Ryzen 7950x3d, 64GB RAM and Linux Mint.How can I improve this? Using external memory is not an option.

image.png

 

 

 

 

 

 My hardware is Ryzen 7950X3D, 64GB RAM and Linux Mint. How can I improve this?

STM32CubeIDE
Version: 1.17.0
Build: 23558_20241125_2245 (UTC)
OS: Linux, v.5.15.0-105-generic, x86_64 / gtk 3.24.33
Java vendor: Eclipse Adoptium
Java runtime version: 21.0.3+9-LTS
Java version: 21.0.3

This topic has been closed for replies.