2022-11-21 06:46 AM
Hello,
I'm controlling a BLDC motor with MCSDK 6.0.0 and IHM08M1, with FOC with 1024 PPR encoder. I compute torque (Iq_ref) commands to achieve speed control, this works ok except in rare case described below:
Sometimes the MCSDK seems "stalled":
Why such behaviour could appear ?
Any clue ?
NB: this seems to occurs when I set a torque command to move the motor starting from 0 rpm.
Thanks,
2022-11-24 06:30 AM
Hello,
Did you check that, after your torque (Iq_ref) command, the internal I_Q_REF register is set accordingly? You can display it with the motor pilot register tab...
What is the control board type?
Best regards.
GMA