2023-10-17 06:32 AM - last edited on 2024-05-29 04:52 AM by GMA
The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enable users to configure their motor-control application and produce a software project that implements it following its hardware component features.
A new documentation will arrive soon and will detail these features:
Current Sensing: three-shunt-raw-currents-differential-internal-opamp-with-external-gain-and-filtered-adc-intput-hwv
ICS
Phase Voltage sensing feature
Driver Protection feature
The descVersion property is equal to 4 from version 6.2.0 of the MCSDK and the "contentVersion" property is added.
For questions regarding the board manager, please respond under this post.
Regards
2023-10-20 06:48 AM
Hi Zied,
good news... we appreciate configuring our custom boards more easily...
However, when we are looking on version 6.2 we don't see the window as shown in the wiki see attached.
Thanks in advance for helping us.
Kind Regards#
Guenther
here the doc window:
thats what we are seeing on 6.2
2023-10-24 05:18 AM
hi @Gboost ,
The interface changes a little, but the parameters remain the same, the same functionalities are offered to the user.
Regards
2023-12-20 02:29 AM
What's the ETA on descVersion 4 of the documentation?