2024-01-11 11:39 AM - edited 2024-01-12 03:24 AM
Hello;
I want to create Ac induction motor project. So I cannot find ACIM GUI or ACIM profile in MC Workbench any versions. Could you please give an answer for my questions
1. Can i download ACIM GUI ?
2. Can i find a acim profile for mc workbench
3. How do i put Acim Selni Ahv 242 to my project
Regards
Motor Workbench 6.2.1
Stm32cubemx 6.10.0
Control board: NUCLEO-G431RB
Power Board: STEVAL-IPM30B
2024-01-15 05:47 AM
Hello @ariftukel ,
Our ACIM offers is currently limited to the following configuration: NUCLEO-G431RB and STEVAL-IHM023V3.
It can be run only through the example list as highlighted below.
We plan to add the full support of the ACIM algorithm for September 2024.
Regards
Cedric
2024-01-21 09:36 AM
Thank you for everything . I will try with them.