cancel
Showing results for 
Search instead for 
Did you mean: 

AC induction Motor for New Project

ariftukel
Associate

Hello;

I want to create  Ac induction motor project. So I cannot find ACIM GUI or ACIM profile in MC Workbench any versions. Could you please give an answer for my questions

1. Can i download ACIM GUI ?

2. Can i find a acim profile  for mc workbench 

3. How do i put Acim Selni Ahv 242 to my project 

Regards 

Motor Workbench  6.2.1

Stm32cubemx 6.10.0

Control board: NUCLEO-G431RB

Power Board: STEVAL-IPM30B

4 REPLIES 4
cedric H
ST Employee

Hello @ariftukel ,

Our ACIM offers is currently limited to the following configuration: NUCLEO-G431RB and STEVAL-IHM023V3.

It can be run only through the example list as highlighted below.

cedricH_0-1705326169109.png

We plan to add the full support of the ACIM algorithm for September 2024.

Regards

Cedric

ariftukel
Associate

Thank you for everything . I will try with them.

 Hi, what is the status for adding the full support of the ACIM algorithm plan? When will it be added? sorry for bad eng :) thx.

Hello Demir42,

I am sorry to inform you that full ACIM support has been postponed. Though it is still on our roadmap, I cannot give you any precise information on when it will be released.

We apologise for the inconvenience.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.