STM32 MCUs Machine learning & AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Edge AI for all. NanoEdge AI Studio autoML tool, now free for STM32 and open to all ARM Cortex-M bas

NanoEdge AI Studio v4.3 is now offered for free to all engineers, giving them the opportunity to create highly efficient TinyML libraries that can be deployed on Cortex-M based microcontrollers. In addition, other enhancements have been integrated to...

ST30449_nanoedge-ai-studio-motor (2).jpg ST30449_nanoedge-ai-studio-motor (2).jpg

Hello. I am developing a device to get optical sensor data(about 10KB) and predict. And this device is portable, so power consumption should be considered. STLinux can be a solution? and which board is suggestable? Thanks. GB

I am a SW engineer, so I ordered HW devp. to others.They are using STM32F4 board to gather optical sensor data and display prediction(sensor requires over 200 KHz reliable clock freq. at minimum).For prediction data will be transfered to phone via bl...

GYoon.1 by Associate II
  • 238 Views
  • 5 replies
  • 0 kudos

trying to run an AI validation project.

Hello,I am using stm32l476, i am trying to run an AI validation project.i replaced the UART with USB (CDC profile)but, when trying to run "validation on target" from the CubeMX, i get this message -> LOAD ERROR: STM32 - no connected board(s), invalid...

AA.10 by Associate III
  • 293 Views
  • 3 replies
  • 0 kudos

AI Pack

Hi,I am using stm32l476, i am trying to run an AI validation project.i replaced the UART with USB (CDC profile)but, when trying to run "validation on target" from the CubeMX, i get this message ->"unable to open the port".In debug mode , i can see th...

AA.10 by Associate III
  • 143 Views
  • 0 replies
  • 0 kudos

Resolved! While analyzing the model with STM32 AI (GUI), confronted a "TOOL ERROR: (1, 4, 12, 10) is not a permutation for (2, 0, 1)"

I confronted an error "TOOL ERROR:  (1, 4, 12, 10) is not a permutation for (2, 0, 1)"It seems there's some issues with handling the model structure. But I can't figure it out.The model perfectly works on python and the structure is not so different ...