When CubeAI is added to the project the .elf file is deleted and not created
I have created a project which uses the Nucleo-H7A3ZI-Q. When I build the project is completed successfully.I then add the software package CUBE-AI version 7.2.0 9 (validation selected) to the project. If I do not upload a network model, then I a war...