STM32 MCUs Machine learning & AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Edge AI for all. NanoEdge AI Studio autoML tool, now free for STM32 and open to all ARM Cortex-M bas

NanoEdge AI Studio v4.3 is now offered for free to all engineers, giving them the opportunity to create highly efficient TinyML libraries that can be deployed on Cortex-M based microcontrollers. In addition, other enhancements have been integrated to...

ST30449_nanoedge-ai-studio-motor (2).jpg ST30449_nanoedge-ai-studio-motor (2).jpg

Validating custom dataset on STM32 X AI.

HiI am following this material to start using STM32 for AI. I have got to the data validation step on page 29 of the document. It works fine while validating using random numbers.But while trying to validate using the dataset, I get the error: TOOL E...

AS.4 by Associate
  • 404 Views
  • 3 replies
  • 1 kudos

STM32CubeMX, X-CUBE-AI error occurring from analysis of prebuilt .tflite network [AI:network] NOT IMPLEMENTED: Unsupported code generation for layer 'Detection' [AI:network] Analyze fail on the AI model

Hi all,Currently using the STM32H747I-DISCO with camera to explore using computer vision for people detection. I have already successfully used one of the example NN (found in the FP-VISION-AI1) and now look to use the X-Cube-AI to integrate further ...

0693W000006ElCkQAK.png
GWall.2 by Associate II
  • 371 Views
  • 1 replies
  • 0 kudos

Hello. I am developing a device to get optical sensor data(about 10KB) and predict. And this device is portable, so power consumption should be considered. STLinux can be a solution? and which board is suggestable? Thanks. GB

I am a SW engineer, so I ordered HW devp. to others.They are using STM32F4 board to gather optical sensor data and display prediction(sensor requires over 200 KHz reliable clock freq. at minimum).For prediction data will be transfered to phone via bl...

GYoon.1 by Associate II
  • 229 Views
  • 5 replies
  • 0 kudos

trying to run an AI validation project.

Hello,I am using stm32l476, i am trying to run an AI validation project.i replaced the UART with USB (CDC profile)but, when trying to run "validation on target" from the CubeMX, i get this message -> LOAD ERROR: STM32 - no connected board(s), invalid...

AA.10 by Associate III
  • 289 Views
  • 3 replies
  • 0 kudos