STM32 MCUs Machine learning & AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Running an AI model in Low-Power?

Hi,I'm working on an application on a STM32WB55 which is sampling sensor data with 52Hz and feed it into a Keras model. Both the raw sampling sensor data as the output of the model will be saved to external flash memory (every 64 samples). A 52Hz int...

F F by Associate II
  • 48 Views
  • 1 replies
  • 0 kudos

SensorTile - SD card is missing

Hello.I evaluate the SensorTile Kit with the following combinations.Core system STLCS01V1Cradle expansion STLCX01V1​When I connect to the Android app "ST BLE Sensor" and select "AI Data Log" to collect learning data, I get an error saying "SD Card is...

gocchan by Associate III
  • 36 Views
  • 0 replies
  • 0 kudos