cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with HALEx RTC Libraries

danirpg
Associate

Hi,

I see a problem in the HAL_RTCCEx_DisableBypassShadow function as the previous post POST advise, they convert the mas to uint8_t and by doing this when the value is and'ed the 24bit on the left are erased unintended.

danirpg_0-1723590891383.png

Im using 1.16.0 of IDE and (STM32Cube MCU Package for STM32H7) 1.11.2 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @danirpg and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Thank you for reporting this. I've escalated to the concerned team for correction on the coming version of the STM32CubeH7 (under internal ticket number 188682).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @danirpg and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Thank you for reporting this. I've escalated to the concerned team for correction on the coming version of the STM32CubeH7 (under internal ticket number 188682).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.