User Activity

Hi,Im starting a new application on a custom board with a STM32H753ZIT, i see when added the FATFS lib from middleware the version of elmchan version is the R0.12c but i see also in the git of the stm32 STM32 FATFS GIT a release of the R0.15 but in t...
Hi,I see a problem in the HAL_RTCCEx_DisableBypassShadow function as the previous post POST advise, they convert the mas to uint8_t and by doing this when the value is and'ed the 24bit on the left are erased unintended.Im using 1.16.0 of IDE and (STM...