2020-05-29 8:18 PM
While debugging my FMC interface I came across what look like errors to me in logic / arithmetic in the stm32f7xx_ll_fmc file.
Here are the two functions of interest to me:
/**
* @brief Initialize the FMC_NORSRAM device according to the specified
* control parameters in the FMC_NORSRAM_InitTypeDef
* @param Device Pointer to NORSRAM device instance
* @param Init Pointer to NORSRAM Initialization structure
* @retval HAL status
*/
HAL_StatusTypeDef FMC_NORSRAM_Init(FMC_NORSRAM_TypeDef *Device, FMC_NORSRAM_InitTypeDef* Init)
{
uint32_t tmpr = 0;
/* Check the parameters */
assert_param(IS_FMC_NORSRAM_DEVICE(Device));
assert_param(IS_FMC_NORSRAM_BANK(Init->NSBank));
assert_param(IS_FMC_MUX(Init->DataAddressMux));
assert_param(IS_FMC_MEMORY(Init->MemoryType));
assert_param(IS_FMC_NORSRAM_MEMORY_WIDTH(Init->MemoryDataWidth));
assert_param(IS_FMC_BURSTMODE(Init->BurstAccessMode));
assert_param(IS_FMC_WAIT_POLARITY(Init->WaitSignalPolarity));
assert_param(IS_FMC_WAIT_SIGNAL_ACTIVE(Init->WaitSignalActive));
assert_param(IS_FMC_WRITE_OPERATION(Init->WriteOperation));
assert_param(IS_FMC_WAITE_SIGNAL(Init->WaitSignal));
assert_param(IS_FMC_EXTENDED_MODE(Init->ExtendedMode));
assert_param(IS_FMC_ASYNWAIT(Init->AsynchronousWait));
assert_param(IS_FMC_WRITE_BURST(Init->WriteBurst));
assert_param(IS_FMC_CONTINOUS_CLOCK(Init->ContinuousClock));
assert_param(IS_FMC_WRITE_FIFO(Init->WriteFifo));
assert_param(IS_FMC_PAGESIZE(Init->PageSize));
/* Get the BTCR register value */
tmpr = Device->BTCR[Init->NSBank];
/* Clear MBKEN, MUXEN, MTYP, MWID, FACCEN, BURSTEN, WAITPOL, WAITCFG, WREN,
WAITEN, EXTMOD, ASYNCWAIT, CBURSTRW and CCLKEN bits */
tmpr &= ((uint32_t)~(FMC_BCR1_MBKEN | FMC_BCR1_MUXEN | FMC_BCR1_MTYP | \
FMC_BCR1_MWID | FMC_BCR1_FACCEN | FMC_BCR1_BURSTEN | \
FMC_BCR1_WAITPOL | FMC_BCR1_CPSIZE | FMC_BCR1_WAITCFG | \
FMC_BCR1_WREN | FMC_BCR1_WAITEN | FMC_BCR1_EXTMOD | \
FMC_BCR1_ASYNCWAIT | FMC_BCR1_CBURSTRW | FMC_BCR1_CCLKEN | FMC_BCR1_WFDIS));
/* Set NORSRAM device control parameters */
tmpr |= (uint32_t)(Init->DataAddressMux |\
Init->MemoryType |\
Init->MemoryDataWidth |\
Init->BurstAccessMode |\
Init->WaitSignalPolarity |\
Init->WaitSignalActive |\
Init->WriteOperation |\
Init->WaitSignal |\
Init->ExtendedMode |\
Init->AsynchronousWait |\
Init->WriteBurst |\
Init->ContinuousClock |\
Init->PageSize |\
Init->WriteFifo);
if(Init->MemoryType == FMC_MEMORY_TYPE_NOR)
{
tmpr |= (uint32_t)FMC_NORSRAM_FLASH_ACCESS_ENABLE;
}
Device->BTCR[Init->NSBank] = tmpr;
/* Configure synchronous mode when Continuous clock is enabled for bank2..4 */
if((Init->ContinuousClock == FMC_CONTINUOUS_CLOCK_SYNC_ASYNC) && (Init->NSBank != FMC_NORSRAM_BANK1))
{
Device->BTCR[FMC_NORSRAM_BANK1] |= (uint32_t)(Init->ContinuousClock);
}
if(Init->NSBank != FMC_NORSRAM_BANK1)
{
Device->BTCR[FMC_NORSRAM_BANK1] |= (uint32_t)(Init->WriteFifo);
}
return HAL_OK;
}
/**
* @brief Initialize the FMC_NORSRAM Timing according to the specified
* parameters in the FMC_NORSRAM_TimingTypeDef
* @param Device Pointer to NORSRAM device instance
* @param Timing Pointer to NORSRAM Timing structure
* @param Bank NORSRAM bank number
* @retval HAL status
*/
HAL_StatusTypeDef FMC_NORSRAM_Timing_Init(FMC_NORSRAM_TypeDef *Device, FMC_NORSRAM_TimingTypeDef *Timing, uint32_t Bank)
{
uint32_t tmpr = 0;
/* Check the parameters */
assert_param(IS_FMC_NORSRAM_DEVICE(Device));
assert_param(IS_FMC_ADDRESS_SETUP_TIME(Timing->AddressSetupTime));
assert_param(IS_FMC_ADDRESS_HOLD_TIME(Timing->AddressHoldTime));
assert_param(IS_FMC_DATASETUP_TIME(Timing->DataSetupTime));
assert_param(IS_FMC_TURNAROUND_TIME(Timing->BusTurnAroundDuration));
assert_param(IS_FMC_CLK_DIV(Timing->CLKDivision));
assert_param(IS_FMC_DATA_LATENCY(Timing->DataLatency));
assert_param(IS_FMC_ACCESS_MODE(Timing->AccessMode));
assert_param(IS_FMC_NORSRAM_BANK(Bank));
/* Get the BTCR register value */
tmpr = Device->BTCR[Bank + 1];
/* Clear ADDSET, ADDHLD, DATAST, BUSTURN, CLKDIV, DATLAT and ACCMOD bits */
tmpr &= ((uint32_t)~(FMC_BTR1_ADDSET | FMC_BTR1_ADDHLD | FMC_BTR1_DATAST | \
FMC_BTR1_BUSTURN | FMC_BTR1_CLKDIV | FMC_BTR1_DATLAT | \
FMC_BTR1_ACCMOD));
/* Set FMC_NORSRAM device timing parameters */
tmpr |= (uint32_t)(Timing->AddressSetupTime |\
((Timing->AddressHoldTime) << 4) |\
((Timing->DataSetupTime) << 8) |\
((Timing->BusTurnAroundDuration) << 16) |\
(((Timing->CLKDivision)-1) << 20) |\
(((Timing->DataLatency)-2) << 24) |\
(Timing->AccessMode)
);
Device->BTCR[Bank + 1] = tmpr;
/* Configure Clock division value (in NORSRAM bank 1) when continuous clock is enabled */
if(HAL_IS_BIT_SET(Device->BTCR[FMC_NORSRAM_BANK1], FMC_BCR1_CCLKEN))
{
tmpr = (uint32_t)(Device->BTCR[FMC_NORSRAM_BANK1 + 1] & ~(((uint32_t)0x0F) << 20));
tmpr |= (uint32_t)(((Timing->CLKDivision)-1) << 20);
Device->BTCR[FMC_NORSRAM_BANK1 + 1] = tmpr;
}
return HAL_OK;
}
The lines of concern for me are lines 42 and 109.
At line 109, each field of the FMC_NORSRAM_TimingTypeDef struct is shifted appropriately for the corresponding FMC_BTRx register parameters (AddressSetupTime is FMC_BTRx[7:4], DataSetupTime is FMC_BTRx[15:8], etc).
But AccessMode is BTRx[29:28], and in the above code AccessMode is not bit-shifted at all, it is just bitwise OR'd with all the other fields from position 0?
And at line 42, none of the fields of the FMC_NORSRAM_TypeDef struct are bit-shifted!
I am pretty sure either both of these or at least one of these instances is a bug, but maybe I am missing something about the implementation? My code runs fine with the above as-is, but that's because almost all of the fields for my particular case are "don't care"s. I have no idea how this file holds for more nuanced interfaces.
2020-05-29 10:28 PM
ST is not careful in defining constants to be used for these functions or macros. Sometimes they are already shifted when defined, sometimes they are not. Find their definitions and check there.
JW
2020-06-05 8:57 AM
Hi @NNagy.1 ,
I shared internally your feedback with our development team for a deeper review.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-06-05 10:54 AM
Aren't all the parameters suitably defined and constructed? Think you're jumping to the wrong conclusions.
/** @defgroup FMC_Access_Mode FMC Access Mode
* @{
*/
#define FMC_ACCESS_MODE_A ((uint32_t)0x00000000U)
#define FMC_ACCESS_MODE_B ((uint32_t)0x10000000U)
#define FMC_ACCESS_MODE_C ((uint32_t)0x20000000U)
#define FMC_ACCESS_MODE_D ((uint32_t)0x30000000)