2024-07-08 07:14 AM
1. CubeMX only allows HAL or LL for SPI and other peripherals. STM32C031C6 itself provides the good SPI clock rate.
SPI LL API function only allows two-byte R/W.. The slave STPM34 Meter IC requires 4-Byte SPI R/W. So we have to choose HAL SPI API calls, such as HAL_SPI_TransmitReceive().
However HAL introduces a big delay (15 us or more) between two consecutive HAL SPI-API calls. We need 6 SPI-API calls within 128us for our application, This big delay inserted by HAL makes it impossible. .
2. The only solution is to write the register low level SPI R/W functions. Is it possible to write it under the current CubeMx IDE compiler for STM32C031C6? Could you provide us the solutions?
Thanks,
Rong
2024-07-16 12:26 AM
I need your help with correcting my the register based SPI code.
The SPI Master is STM32C031C6 Nucleo Eva board.
The SPI Slave is STPM34 (Meter IC) Eva Board.
Test Result:
1. The HAL Function HAL_SPI_TransmitReceive(...) works, but introduces a long delay.
2. I tried to write the register based SPI code to do the same as the above HAL function, but it does not work.
Could you make some correction on the code below? Or provide me with some working code? Thank you very much!
void SPI_Transmit_Receive (const uint8_t *data_tx, uint8_t *data_rx, uint8_t size)
{
uint8_t size1 = size;
SPI1->CR1 |= (1u << 6); //ENABLE SPI
while (size)
{
if (size == size1)
{
if (__HAL_SPI_GET_FLAG(&hspi1, SPI_FLAG_TXE))
{
SPI1->DR = *((uint16_t *)data_tx);
data_tx += sizeof(uint16_t);
size -= 2U;
}
}
if (size1 > size)
{
if (__HAL_SPI_GET_FLAG(&hspi1, SPI_FLAG_RXNE))
{
* (uint16_t *)data_rx = (uint16_t)SPI1->DR;
data_rx += sizeof(uint16_t);
size1 -= 2U;
}
}
}
SPI1->CR1 &= ~(1u << 6); //DISABLE SPI
}
2024-07-16 01:55 AM
There's that echo again!
Please see the instructions to properly post source code:
2024-07-16 03:50 AM - edited 2024-07-16 03:57 AM
Hello @RongShengWang ,
Is the data size set to greater than SPI_DATASIZE_8BIT? If yes, could you please try with this code?
void SPI_Transmit_Receive(const uint8_t *data_tx, uint8_t *data_rx, uint8_t size)
{
uint8_t rx_size= size;
uint8_t tx_size = size;
/* Set the Rx Fifo threshold */
if (size > 1U)
{
/* Set fiforxthreshold according the reception data length: 16bit */
CLEAR_BIT(SPI1->CR2, SPI_RXFIFO_THRESHOLD);
}
/* Enable SPI */
SPI1->CR1 |= SPI_CR1_SPE;
while (size > 0)
{
/* Wait until TXE (Transmit buffer empty) flag is set */
while (!__HAL_SPI_GET_FLAG(&hspi1, SPI_FLAG_TXE));
/* Transmit data */
if (tx_size > 1U)
{
SPI1->DR = *((uint16_t *)data_tx);
data_tx += sizeof(uint16_t);
tx_size -= 2U;
}
else
{
*(__IO uint8_t *)&SPI1->DR = (*data_tx);
data_tx ++;
tx_size --;
}
/* Wait until RXNE (Receive buffer not empty) flag is set */
while (!__HAL_SPI_GET_FLAG(&hspi1, SPI_FLAG_RXNE));
if (rx_size > 1U)
{
*((uint16_t *)data_rx) = (uint16_t)SPI1->DR;
data_rx += sizeof(uint16_t);
rx_size -= 2U;
if (rx_size <= 1U)
{
/* Set RX Fifo threshold before to switch on 8 bit data size */
SET_BIT(SPI1->CR2, SPI_RXFIFO_THRESHOLD);
}
}
else
{
(*(uint8_t *)data_rx) = *(__IO uint8_t *)&SPI1->DR;
data_rx++;
rx_size --;
}
}
/* Wait until the SPI is not busy */
while (__HAL_SPI_GET_FLAG(&hspi1, SPI_FLAG_BSY));
/* Disable SPI */
SPI1->CR1 &= ~SPI_CR1_SPE;
}
2024-07-16 05:00 AM
Hi, Omar,
Thank you very much for your timely help. I found my setting is -
hspi1.Init.DataSize = SPI_DATASIZE_8BIT; - Was it a big problem with my code?
Should I change it to hspi1.Init.DataSize = SPI_DATASIZE_16BIT to run your code?
Thank you very much!
Rong
2024-07-16 05:18 AM
Hi, Omar,
I found my setting is - hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
I also tried to send one byte - 8 bits, rather than 16 bits, at a time. It did not work either.
Should I change it to hspi1.Init.DataSize = SPI_DATASIZE_16BIT to run your code?
Thank you very much!
Rong