Hello @TMich.1
STM32 uses little-endian format. Concerning I2S, data are sent MSB first.
I assume that you have configured SAI to perform I2S transfer and set up a frame with 2 slots, each 32 bits per slot.
You also need to configure the data size, ...
Hello @TNaum
Your issue has been reported internally. We will come back to you as soon as possible.
Internal ticket number: 189257 (This is an internal tracking number and is not accessible or usable by customers)
Hello @Anusree_k
what is the size of the data to be read?
The reload mode is used when the data size to be read is greater than 255, however it is mandatory to call LL_I2C_HandleTransfer with LL_I2C_MODE_AUTOEND mode for the last amount of data l...